<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 AFX Load Utility?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528632#M1047</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by scs on Thu Jan 26 09:37:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, I meant AXF Load Utility.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any way to load a &amp;lt;project&amp;gt;.AXF file (or some other objcopy format for an old CodeRed project build) to an LPCXpresso board via USB without using the CodeRed IDE's "Debug" command?&amp;nbsp; Such as a command line program, CodeRed IDE command, or separate Windows application?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:53:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:53:39Z</dc:date>
    <item>
      <title>AFX Load Utility?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528632#M1047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by scs on Thu Jan 26 09:37:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, I meant AXF Load Utility.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any way to load a &amp;lt;project&amp;gt;.AXF file (or some other objcopy format for an old CodeRed project build) to an LPCXpresso board via USB without using the CodeRed IDE's "Debug" command?&amp;nbsp; Such as a command line program, CodeRed IDE command, or separate Windows application?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528632#M1047</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: AFX Load Utility?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528633#M1048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_USA on Thu Jan 26 09:51:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There is a flash programming utility built into LPCXpresso. It can be found on the icon bar. It looks like a chip.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528633#M1048</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:41Z</dc:date>
    </item>
    <item>
      <title>Re: AFX Load Utility?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528634#M1049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Jan 26 09:53:51 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Command line?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/AFX-Load-Utility/m-p/528634#M1049</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:41Z</dc:date>
    </item>
  </channel>
</rss>