<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Problem with Win7 and LPCXpresso</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547861#M10266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sat Oct 08 15:55:24 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Under xp it is booted as a winusb device but under win7 it is booted as a hid device, so you will find it under hid devices. There is a preference for changing this. Afaik it is done like this for performance reasons as the xp hid device driver is c***.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:23:34 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:23:34Z</dc:date>
    <item>
      <title>Problem with Win7 and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547858#M10263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Fri Oct 07 07:55:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have installed Win7 64-bit (perhaps a mistake) on my system previously running XP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Previously, LPCXpresso worked fine.&amp;nbsp;&amp;nbsp; Now I cannot get the connection to&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the LPCXpresso pod to work properly.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working with a 1114/301.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have followed the diagnostic here;&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/LPCLinkDiagnostics&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I plug the pod in I see "USB Device with DFU Capabilities" using&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Device Manager.&amp;nbsp;&amp;nbsp; When I execute "bootLPCXpresso hid" the DFU device&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;disappears and two new devices appear in "Human Interface Devices".&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The new devices are "HID-compliant device" and "USB Input Device".&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hewever these new devices do not appear to be the LPCXpresso judging&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;from the hardware ID's.&amp;nbsp;&amp;nbsp; It seems that the LPCXpresso has disappeared!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I unplug it the above cycle repears.&amp;nbsp;&amp;nbsp; I never see LPC-Link as I did&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;with XP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there anything that I can do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pete.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547858#M10263</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:23:32Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Win7 and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547859#M10264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Fri Oct 07 08:27:53 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Win7 64-bit works OK here. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What happens when you let LPCXpresso do its own booting? If there is a problem it gives you the option to display the log. What does that show you?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547859#M10264</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Win7 and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547860#M10265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Sat Oct 08 09:00:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I solved the problem.&amp;nbsp;&amp;nbsp; My fault.&amp;nbsp;&amp;nbsp; When I installed Win7 I also installed a clean copy of LPCXpresso V4.1.0_190 and CMSISv2p00_LPC11xx which got me a new system_LPC11xx.c file.&amp;nbsp;&amp;nbsp; This contains;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=#3f7f5f][COLOR=#3f7f5f]#define SYSPLLCLKSEL_Val&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000001[/COLOR][/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=#3f7f5f][COLOR=#3f7f5f][COLOR=black]which selects an extrnal oscillator.&amp;nbsp;&amp;nbsp; I am using the internal oscillator so this causes [/COLOR][COLOR=black]a hang in the wait until PLL locked loop.&amp;nbsp;&amp;nbsp; I had fixed this in my old environment but [/COLOR][COLOR=#000000]the new environment killed me.&amp;nbsp;&amp;nbsp; So this was my fault.[/COLOR][/COLOR][/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=#000000]What threw me was that under XP the LPC pod appears as "LPC Link" in device manager when LPCXpresso had initialized the pod.&amp;nbsp;&amp;nbsp; Under Win7 it just disappears after initialization![/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pete.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547860#M10265</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Win7 and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547861#M10266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sat Oct 08 15:55:24 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Under xp it is booted as a winusb device but under win7 it is booted as a hid device, so you will find it under hid devices. There is a preference for changing this. Afaik it is done like this for performance reasons as the xp hid device driver is c***.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-Win7-and-LPCXpresso/m-p/547861#M10266</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:23:34Z</dc:date>
    </item>
  </channel>
</rss>