<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART echo help!!! in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-echo-help/m-p/547206#M10007</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Wed Aug 04 01:58:17 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You do realise that there is actually a UART example provided with the NXP LPCXpresso1114 examples?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, if you want to test your code, then I would suggest running it! ;) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You will either need to add a serial connector to your LPCXpresso board, or else you could plug your LPCXPresso board onto the baseboard that is available from Embedded Artists:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php?PHPSESSID=7j4kdsgi90apad92h5m5jjq8v3&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupprot&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:03:24 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:03:24Z</dc:date>
    <item>
      <title>UART echo help!!!</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-echo-help/m-p/547205#M10006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by zeal007 on Tue Aug 03 03:06:02 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]good day everyone,[/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]I used the ser_Write and ser_Read of LPC1343 examples to have a simple UART_echo using the LPC1114. It has no error, but I don't know if it really work or shall i say, does it really write to the UART of LPC1114?[/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]My problem now is that, how can i know if it really works, if it is possible to use the ser_Write and ser_Read functions, to the UART of LPC1114?[/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]Or do i miss something importing the functions?[/B]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-echo-help/m-p/547205#M10006</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: UART echo help!!!</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-echo-help/m-p/547206#M10007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Wed Aug 04 01:58:17 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You do realise that there is actually a UART example provided with the NXP LPCXpresso1114 examples?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, if you want to test your code, then I would suggest running it! ;) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You will either need to add a serial connector to your LPCXpresso board, or else you could plug your LPCXPresso board onto the baseboard that is available from Embedded Artists:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php?PHPSESSID=7j4kdsgi90apad92h5m5jjq8v3&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupprot&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-echo-help/m-p/547206#M10007</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:03:24Z</dc:date>
    </item>
  </channel>
</rss>