<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: 1769 refuses to start</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547202#M10003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 13:54:43 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Replaced cap with 10nf and starts reliably. !! Happy !!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:55:12 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:55:12Z</dc:date>
    <item>
      <title>1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547194#M9995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 05:59:03 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;So after a couple months testing on breadboards with the help of breakouts, I've made a PCB for my 1769 project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In this board, I only use 1x 12Mhz crystal. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is no 32768khz xtal2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For some strange reason, when I power up the board from the onboard USB socket -&amp;gt; into the onboard&amp;nbsp; 5v to 3v3 LDO to power the board, the processor refuses to start.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have to do a manual reset ( RESET_N to GND ) and then the board starts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When it is already powered up from USB and I re-program from the JTAG/SWD, it starts normally and works normally as if I was still using the original LPCXpresso board and breakouts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The pins relevant are, as far as I know, all connected properly:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;+3v3 : Pins 10, 12, 19, 28, 42, 54, 71, 84, 96&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;GND: Pins 11, 15, 31, 41, 55, 72, 83, 97&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then also...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1) a 10K resistor from pin 4 TRST_N (pin 4)&amp;nbsp; to +3v3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) a 10K resistor from pin 17 RESET_N (pin17)&amp;nbsp; to +3v3&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Where could I be wrong, and what to test to know if the board is holding in reset for some reason.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Last but not least. Pullups on JTAG are not fitted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Edit: fitted a 100nF to ground on the RESET_N, to try a delay.... still no joy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks !!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547194#M9995</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547195#M9996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sun Jul 24 06:39:19 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Pin13 :confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pin 53 :confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LDO circuit ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;JTAG connected or SWD connected ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547195#M9996</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547196#M9997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 07:29:32 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Pin 13 is not connected to anything.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pin 53 has a push switch connected to it. Pin 53 is tied to high with a 10K pullup and also a 100nf for debounce.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This serves as UART0 bootloader mode entry if kept pressed on powerup. ( FlashMagic )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LDO... LM1117 3v3. 10uf on input, 10uf+100nf on output.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;JTAG connected or SWD connected ?&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;I'm using an extension of the LPCXpresso programming pins into my board.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547196#M9997</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547197#M9998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sun Jul 24 07:42:58 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you check if all pins are really connected ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you check your crystal (could be a little bit slow) and it's caps ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does this problem occur with and without connected SWD ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does this problem occur if you use a 5V power supply instead USB ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547197#M9998</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547198#M9999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 13:29:08 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Zero, Thanks for your reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;Did you check if all pins are really connected ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I did again a thorough check on all supply, gnd, RESET_N and TRST_N, and also their pullups. 100% good.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;Did you check your crystal (could be a little bit slow) and it's caps ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The crystal timing confirmed 12.000Mhz ( same components from the LPCXpresso board )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;Does this problem occur with and without connected SWD ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Absolutely. With and without... same No Startup, unless I manually reset RESET_N, where it then starts up as normal.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've even tried some delays in code, on startup, just after SystemInit. No Joy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;Does this problem occur if you use a 5V power supply instead USB ? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes. USB supply, or 5volt into the regulator input produce the same issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hmmm....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What can I do to use RSTOUT_N as a clue to this problem ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any thing in code that I can use ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Debugging to try to see what;s happening is not helpful, because just after a programming, the board always starts perfectly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To me it seems that something is causing the board to jump into bootloader mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Which is the most helpful pdf regarding bootloader on the 1769 ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547198#M9999</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547199#M10000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sun Jul 24 13:45:02 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Wenzu&lt;/STRONG&gt;&lt;BR /&gt;To me it seems that something is causing the board to jump into bootloader mode.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then scope pin 53 to control if it's low too long :confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or use FlashMagic to control if you're in ISP mode :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547199#M10000</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:10Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547200#M10001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 13:48:42 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ok Thanks.. will do.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll try removing the de-bounceing 100nf as well.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547200#M10001</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:10Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547201#M10002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 13:51:54 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That fixes it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks Zero.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Removing the 100nF from Pin53-to-GND makes the board start reliably.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorted. Another 2 beers for you !!:):):)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547201#M10002</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:11Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547202#M10003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 13:54:43 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Replaced cap with 10nf and starts reliably. !! Happy !!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547202#M10003</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547203#M10004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sun Jul 24 14:01:22 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Increasing Reset pullup to something like 20k should work also (with 10k / 100nf @ pin53) :eek::eek:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547203#M10004</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 refuses to start</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547204#M10005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wenzu on Sun Jul 24 14:08:44 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course.... this will delay startup. Thanks for pointing it out.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But I prefer to have the MCU start up as fast as possible, Then I check debounce in code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I really would like to Thank You for your help. I learn something new everytime. This is best education one can have.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-refuses-to-start/m-p/547204#M10005</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:55:13Z</dc:date>
    </item>
  </channel>
</rss>