<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there a feature to do error correction for UARTs on LPC17xx? in LPC FAQs</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/Is-there-a-feature-to-do-error-correction-for-UARTs-on-LPC17xx/m-p/466964#M96</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;The LSR register in UART can detect:&lt;BR /&gt;*) Overrun - Data is missing due to UART RX FIFO is full&lt;BR /&gt;*) Parity error &lt;BR /&gt;*) Framing error - Error if the stop bit is missing&lt;BR /&gt;*) Break Interrupt.- Data is 0x00 (including parity bit)&lt;/P&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;However, UART cannot recover the missing bits from faulty transfer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 14:10:50 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-03-31T14:10:50Z</dc:date>
    <item>
      <title>Is there a feature to do error correction for UARTs on LPC17xx?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/Is-there-a-feature-to-do-error-correction-for-UARTs-on-LPC17xx/m-p/466964#M96</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;The LSR register in UART can detect:&lt;BR /&gt;*) Overrun - Data is missing due to UART RX FIFO is full&lt;BR /&gt;*) Parity error &lt;BR /&gt;*) Framing error - Error if the stop bit is missing&lt;BR /&gt;*) Break Interrupt.- Data is 0x00 (including parity bit)&lt;/P&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;However, UART cannot recover the missing bits from faulty transfer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 14:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/Is-there-a-feature-to-do-error-correction-for-UARTs-on-LPC17xx/m-p/466964#M96</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T14:10:50Z</dc:date>
    </item>
  </channel>
</rss>