<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC FAQs中的主题 When I start debugging (using LPCXpresso, Keil, IAR), I noticed that my program started in the bootROM area (0x1FFF_xxxx) although the program download is done and verification is correct</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/When-I-start-debugging-using-LPCXpresso-Keil-IAR-I-noticed-that/m-p/464718#M68</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;On the MCU, please check if the ISP pin is activated (ie. pulled LOW). Otherwise, every time the JTAG / SWD is reset, the MCU will go into bootROM, instead of the user program.&lt;/P&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;If the ISP pin is not pulled LOW, please check the IDE's configuration. For Keil, the 'Connect' option in Project -&amp;gt;Options for xxx -&amp;gt;Debug-&amp;gt;Settings must be set to 'with pre-reset'. For IAR, set Project-&amp;gt;Options-&amp;gt;Debugger-&amp;gt;"JTAG Name"-&amp;gt;Reset to "Normal". If your project is using an external JTAG configuration (*.ini in Keil and *.mac in IAR), please make sure that it is configured to point to internal Flash or SRAM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 01:47:16 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-03-31T01:47:16Z</dc:date>
    <item>
      <title>When I start debugging (using LPCXpresso, Keil, IAR), I noticed that my program started in the bootROM area (0x1FFF_xxxx) although the program download is done and verification is correct</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/When-I-start-debugging-using-LPCXpresso-Keil-IAR-I-noticed-that/m-p/464718#M68</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;On the MCU, please check if the ISP pin is activated (ie. pulled LOW). Otherwise, every time the JTAG / SWD is reset, the MCU will go into bootROM, instead of the user program.&lt;/P&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;If the ISP pin is not pulled LOW, please check the IDE's configuration. For Keil, the 'Connect' option in Project -&amp;gt;Options for xxx -&amp;gt;Debug-&amp;gt;Settings must be set to 'with pre-reset'. For IAR, set Project-&amp;gt;Options-&amp;gt;Debugger-&amp;gt;"JTAG Name"-&amp;gt;Reset to "Normal". If your project is using an external JTAG configuration (*.ini in Keil and *.mac in IAR), please make sure that it is configured to point to internal Flash or SRAM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 01:47:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/When-I-start-debugging-using-LPCXpresso-Keil-IAR-I-noticed-that/m-p/464718#M68</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T01:47:16Z</dc:date>
    </item>
  </channel>
</rss>