<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC FAQs中的主题 Re: If the LCD controller has a lower priority on the EMC bus, refreshes will be stalled. How noticable is this on the screen?</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/If-the-LCD-controller-has-a-lower-priority-on-the-EMC-bus/m-p/463107#M27</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="comment-id"&gt;#1&lt;/SPAN&gt;Submitted by mahessel on Wed, 2013-08-21 06:00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the solution for this issue? How do I increase this priority?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 17:27:25 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-04-26T17:27:25Z</dc:date>
    <item>
      <title>If the LCD controller has a lower priority on the EMC bus, refreshes will be stalled. How noticable is this on the screen?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/If-the-LCD-controller-has-a-lower-priority-on-the-EMC-bus/m-p/463106#M26</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;If it happens, a DMA underflow will occur causing a tear. For the frame being rendered when this happens, the data under the spot of the display where the tear happen will be misaligned. Because the frame is being updated at a high rate (60Hz?), you see a quick flicker on the display. If the tear happens a lot, the flicker can be annoying.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;It should be noted that the LCD controller will underflow only when it's DMA request is stalled for a considerable amount of time. The LCD controller has it's own buffer memory filled up by DMA and can handle short stalls during it's DMA request.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 00:57:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/If-the-LCD-controller-has-a-lower-priority-on-the-EMC-bus/m-p/463106#M26</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T00:57:07Z</dc:date>
    </item>
    <item>
      <title>Re: If the LCD controller has a lower priority on the EMC bus, refreshes will be stalled. How noticable is this on the screen?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/If-the-LCD-controller-has-a-lower-priority-on-the-EMC-bus/m-p/463107#M27</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="comment-id"&gt;#1&lt;/SPAN&gt;Submitted by mahessel on Wed, 2013-08-21 06:00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the solution for this issue? How do I increase this priority?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 17:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/If-the-LCD-controller-has-a-lower-priority-on-the-EMC-bus/m-p/463107#M27</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-26T17:27:25Z</dc:date>
    </item>
  </channel>
</rss>