<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1347 USB Control Transfer in LPC FAQs</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/LPC1347-USB-Control-Transfer/m-p/637960#M169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our customer SIGMATEK wants to implement USB Control Transfers on the LPC1347. &lt;/P&gt;&lt;P&gt;This works nice as long as they have a data length of less than 64 or more than 64 Bytes.&lt;/P&gt;&lt;P&gt;If the data length is exactly 64 Bytes (or a multiple of 64 bytes) then this does not work anymore.&lt;/P&gt;&lt;P&gt;What do they need to do to get this working??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Feb 2017 08:33:18 GMT</pubDate>
    <dc:creator>peter_furtner</dc:creator>
    <dc:date>2017-02-15T08:33:18Z</dc:date>
    <item>
      <title>LPC1347 USB Control Transfer</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPC1347-USB-Control-Transfer/m-p/637960#M169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our customer SIGMATEK wants to implement USB Control Transfers on the LPC1347. &lt;/P&gt;&lt;P&gt;This works nice as long as they have a data length of less than 64 or more than 64 Bytes.&lt;/P&gt;&lt;P&gt;If the data length is exactly 64 Bytes (or a multiple of 64 bytes) then this does not work anymore.&lt;/P&gt;&lt;P&gt;What do they need to do to get this working??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 08:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPC1347-USB-Control-Transfer/m-p/637960#M169</guid>
      <dc:creator>peter_furtner</dc:creator>
      <dc:date>2017-02-15T08:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1347 USB Control Transfer</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPC1347-USB-Control-Transfer/m-p/2413050#M173</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;When USB data payloads equal an exact multiple of the endpoint's maximum packet size (64 bytes for Full-Speed), the receiver hangs because there is no short packet to signal the end of the transfer; to fix this on the LPC1347, SIGMATEK must check if the payload length is a non-zero multiple of 64 and, if so, manually send a Zero-Length Packet (ZLP) with a length of zero right after the main data block to flush the buffer, signal completion, and successfully terminate the transfer.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2026 10:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPC1347-USB-Control-Transfer/m-p/2413050#M173</guid>
      <dc:creator>dedog57501</dc:creator>
      <dc:date>2026-09-11T10:42:02Z</dc:date>
    </item>
  </channel>
</rss>