<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I see error frames on the CAN bus whenever my code starts up, before the CAN controller is initialized. What is a common reason for this? in LPC FAQs</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/I-see-error-frames-on-the-CAN-bus-whenever-my-code-starts-up/m-p/590993#M164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The most common reason is that the CAN_TX pin has been set to logic zero before the CAN controller is initialized and enabled. Even a brief period can cause a burst of error frames.&lt;BR /&gt;Set the pin state to logic one before setting the CAN_TX pin to be an output. Alternatively, configure and initialize the CAN controller fully before connecting it to the CAN_TX and CAN_RX pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 22:05:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-09-02T22:05:52Z</dc:date>
    <item>
      <title>I see error frames on the CAN bus whenever my code starts up, before the CAN controller is initialized. What is a common reason for this?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/I-see-error-frames-on-the-CAN-bus-whenever-my-code-starts-up/m-p/590993#M164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The most common reason is that the CAN_TX pin has been set to logic zero before the CAN controller is initialized and enabled. Even a brief period can cause a burst of error frames.&lt;BR /&gt;Set the pin state to logic one before setting the CAN_TX pin to be an output. Alternatively, configure and initialize the CAN controller fully before connecting it to the CAN_TX and CAN_RX pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 22:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/I-see-error-frames-on-the-CAN-bus-whenever-my-code-starts-up/m-p/590993#M164</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-09-02T22:05:52Z</dc:date>
    </item>
  </channel>
</rss>