<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I test the CAN peripheral and driver without a CAN transceiver and CAN bus connected? in LPC FAQs</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/How-can-I-test-the-CAN-peripheral-and-driver-without-a-CAN/m-p/590976#M163</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Use the internal loopback feature of the CAN controller. This allows the controller to receive what it transmits without the bus being used. Typically this mode is enabled by setting a bit in the control register before enabling the CAN controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 22:04:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-09-02T22:04:06Z</dc:date>
    <item>
      <title>How can I test the CAN peripheral and driver without a CAN transceiver and CAN bus connected?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/How-can-I-test-the-CAN-peripheral-and-driver-without-a-CAN/m-p/590976#M163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Use the internal loopback feature of the CAN controller. This allows the controller to receive what it transmits without the bus being used. Typically this mode is enabled by setting a bit in the control register before enabling the CAN controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 22:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/How-can-I-test-the-CAN-peripheral-and-driver-without-a-CAN/m-p/590976#M163</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-09-02T22:04:06Z</dc:date>
    </item>
  </channel>
</rss>