<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC FAQs中的主题 What is the sample point for?</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/What-is-the-sample-point-for/m-p/590701#M154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The sample point is the location, typically given as a percent value, inside each bit period where the CAN controller looks at the state of the bus and determines if it is a logic zero (dominant) or logic one (recessive). All CAN controllers allow this point to be configured and it is always specified as a percentage from the start of the bit period.&lt;BR /&gt;The location of the sample point is a trade-off. An early sample point decreases the sensitivity to oscillator tolerances and allows lower-quality oscillators. A late sample point allows for a longer signal propagation time and therefore a longer bus. A later sample point is useful for non-ideal bus topologies.&lt;BR /&gt;The CAN-in-Automation user’s group makes recommendations of where the sample point should be for various bit rates, with 87.5% the most common.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 21:56:55 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-09-02T21:56:55Z</dc:date>
    <item>
      <title>What is the sample point for?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/What-is-the-sample-point-for/m-p/590701#M154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The sample point is the location, typically given as a percent value, inside each bit period where the CAN controller looks at the state of the bus and determines if it is a logic zero (dominant) or logic one (recessive). All CAN controllers allow this point to be configured and it is always specified as a percentage from the start of the bit period.&lt;BR /&gt;The location of the sample point is a trade-off. An early sample point decreases the sensitivity to oscillator tolerances and allows lower-quality oscillators. A late sample point allows for a longer signal propagation time and therefore a longer bus. A later sample point is useful for non-ideal bus topologies.&lt;BR /&gt;The CAN-in-Automation user’s group makes recommendations of where the sample point should be for various bit rates, with 87.5% the most common.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 21:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/What-is-the-sample-point-for/m-p/590701#M154</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-09-02T21:56:55Z</dc:date>
    </item>
  </channel>
</rss>