<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What is CAN-FD? in LPC FAQs</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/What-is-CAN-FD/m-p/590677#M153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CAN-FD is a new CAN bus frame format, developed by Bosch. The current version was also published as&lt;BR /&gt;an international standard ISO 11898-1:2015. It allows for up to 64 bytes of data per frame and&lt;BR /&gt;significantly higher bit rates. Note that the first CAN-FD implementations are referred to as non-ISO&lt;BR /&gt;CAN-FD and should not be used due to flaws in the CRC handling. The ISO version of CAN-FD not only&lt;BR /&gt;fixes the flaws but has an increased hamming distance. With CAN-FD, nodes can transmit more data,&lt;BR /&gt;faster and with improved data integrity, while retaining all other features that make CAN ideal for&lt;BR /&gt;industrial communications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 21:53:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-09-02T21:53:47Z</dc:date>
    <item>
      <title>What is CAN-FD?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/What-is-CAN-FD/m-p/590677#M153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CAN-FD is a new CAN bus frame format, developed by Bosch. The current version was also published as&lt;BR /&gt;an international standard ISO 11898-1:2015. It allows for up to 64 bytes of data per frame and&lt;BR /&gt;significantly higher bit rates. Note that the first CAN-FD implementations are referred to as non-ISO&lt;BR /&gt;CAN-FD and should not be used due to flaws in the CRC handling. The ISO version of CAN-FD not only&lt;BR /&gt;fixes the flaws but has an increased hamming distance. With CAN-FD, nodes can transmit more data,&lt;BR /&gt;faster and with improved data integrity, while retaining all other features that make CAN ideal for&lt;BR /&gt;industrial communications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 21:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/What-is-CAN-FD/m-p/590677#M153</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-09-02T21:53:47Z</dc:date>
    </item>
  </channel>
</rss>