<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC FAQsのトピックHow to detect and handle bus off?</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/How-to-detect-and-handle-bus-off/m-p/590653#M152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bus off means that the transmit error counter (see explanation further down) has reached 256. There&lt;BR /&gt;are many possible causes of this but it could mean that the CAN controller is misconfigured or the&lt;BR /&gt;controller is not connected to the CAN bus. The root cause of the problem should be addressed to stop&lt;BR /&gt;it happening again. For a misconfiguration it could be that the bit rate is incorrect.&lt;BR /&gt;Once in bus off the CAN controller will set a flag in the status register to indicate the state has been&lt;BR /&gt;entered and it is common that CAN controllers also trigger an interrupt.&lt;BR /&gt;Bus off mode traditionally can only be exited by re-initializing the CAN controller, but some newer CAN&lt;BR /&gt;controllers also allow to clear that state individually or even automatically after a certain time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 21:52:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-09-02T21:52:26Z</dc:date>
    <item>
      <title>How to detect and handle bus off?</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/How-to-detect-and-handle-bus-off/m-p/590653#M152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bus off means that the transmit error counter (see explanation further down) has reached 256. There&lt;BR /&gt;are many possible causes of this but it could mean that the CAN controller is misconfigured or the&lt;BR /&gt;controller is not connected to the CAN bus. The root cause of the problem should be addressed to stop&lt;BR /&gt;it happening again. For a misconfiguration it could be that the bit rate is incorrect.&lt;BR /&gt;Once in bus off the CAN controller will set a flag in the status register to indicate the state has been&lt;BR /&gt;entered and it is common that CAN controllers also trigger an interrupt.&lt;BR /&gt;Bus off mode traditionally can only be exited by re-initializing the CAN controller, but some newer CAN&lt;BR /&gt;controllers also allow to clear that state individually or even automatically after a certain time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit &lt;A href="http://www.esacademy.com"&gt;www.esacademy.com&lt;/A&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 21:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/How-to-detect-and-handle-bus-off/m-p/590653#M152</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-09-02T21:52:26Z</dc:date>
    </item>
  </channel>
</rss>