<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC FAQs中的主题 Re: LPCOpen debug input/output support</title>
    <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471315#M115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="submitted"&gt;&lt;SPAN class="comment-id"&gt;#1&lt;/SPAN&gt;Submitted by nicolasberan on Tue, 2014-07-08 22:16.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi, im trying yo change the DEBUGIN() macro, i need to use getchar so i replaced the DEBUGIN() Board_UARTGetChar() with the getchar() but when i do it, the macro seem like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(--(((&amp;amp;__Ciob[0]))-&amp;gt;__icnt) &amp;gt;= 0 ? *(((&amp;amp;__Ciob[0]))-&amp;gt;__ptr)++ : __filbuf((&amp;amp;__Ciob[0])))&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i replace the DEBUGIN() instruction with getchar(), it works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Apr 2016 16:05:56 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-04-22T16:05:56Z</dc:date>
    <item>
      <title>LPCOpen debug input/output support</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471314#M114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPCOpen supports simple debug input/output support as part of the standard board layer API. These functions can be used to provide simple debug message output and input via a UART or device.&amp;nbsp; The functions are abstracted in the board layer and can be reimplemented to another device if needed. Default implementations included with LPCopen use available UARTs for a board if they exist, but can also be routed via semihosting to the debuggers console if it's available. If a UART capability doesn't exist on the board, debug support is usually disabled for that board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is recommended to use the DEBUG* implementations for debug input and output instead of printf or other custom implementations as the functions can easily be removed from an image by simply building the board layer code and example code with DEBUG_ENABLE undefined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H1 id="toc-hId-1904850313"&gt;DEBUG function implementations&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Inlcuded as part of the common board API in the 'lpcopen/software/lpc_core/\lpc_board/board_common' area, the board_api.h file includes the default DEBUG* implementation and functions used by all LPCOpen boards. If you want to replace the functions for your platform, you can change this file to use your own implementations. The selected implementation of the DEBUG* functions depend on the enabled states of the DEBUG_ENABLE and DEBUG_SEMIHOSTING definitions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPCOpen DEBUG* functions defined in the board_api.h file are &lt;STRONG&gt;DEBUGINIT&lt;/STRONG&gt;(), &lt;STRONG&gt;DEBUGOUT&lt;/STRONG&gt;(), &lt;STRONG&gt;DEBUGSTR&lt;/STRONG&gt;(), and &lt;STRONG&gt;DEBUGIN&lt;/STRONG&gt;(). These are defined as macro definitions that select a specific implementation based on whether DEBUG_ENABLE and DEBUG_SEMIHOSTING are defined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code used for this is shown below. &lt;EM&gt;This code may change over time, see the board_api.h file for the latest implementation.&lt;/EM&gt;&lt;/P&gt;&lt;PRE class="jive-pre"&gt;/* The DEBUG* functions are selected based on system configuration.&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&amp;nbsp;&amp;nbsp; Code that uses the DEBUG* functions will have their I/O routed to
&amp;nbsp;&amp;nbsp; the UART, semihosting, or nowhere. */
#if defined(DEBUG_ENABLE)
#if defined(DEBUG_SEMIHOSTING)
#define DEBUGINIT()
#define DEBUGOUT(...) printf(__VA_ARGS__)
#define DEBUGSTR(str) printf(str)
#define DEBUGIN() (int) EOF

#else
#define DEBUGINIT() Board_Debug_Init()
#define DEBUGOUT(...) printf(__VA_ARGS__)
#define DEBUGSTR(str) Board_UARTPutSTR(str)
#define DEBUGIN() Board_UARTGetChar()
#endif /* defined(DEBUG_SEMIHOSTING) */

#else
#define DEBUGINIT()
#define DEBUGOUT(...)
#define DEBUGSTR(str)
#define DEBUGIN() (int) EOF
#endif /* defined(DEBUG_ENABLE) */&lt;/PRE&gt;&lt;H2 id="toc-hId--843820153"&gt;&lt;/H2&gt;&lt;H2 id="toc-hId-898990182"&gt;&lt;SPAN style="color: #eb7a3d;"&gt;DEBUG_ENABLE and DEBUG_SEMIHOSTING definitions&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Define or undefine the DEBUG_ENABLE and DEBUG_SEMIHOSTING definitions to disable DEBUG* functions complete or enable debugging via a device (UART) or via semihosting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When both DEBUG_ENABLE and DEBUG_SEMIHOSTING are undefined, DEBUG* functions will be built out of the code and make a much smaller image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When DEBUG_ENABLE is defined and DEBUG_SEMIHOSTING is undefined, DEBUG* functions will be setup for the default device. For supported LPCOpen boards, this is usually a UART. The default UART implementations of &lt;STRONG&gt; DEBUGOUT&lt;/STRONG&gt;() and &lt;STRONG&gt;DEBUGSTR&lt;/STRONG&gt;() functions are blocking and will affect code timing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When both DEBUG_ENABLE and DEBUG_SEMIHOSTING are defined, DEBUG* functions will be setup for semihosting. This capability varies per toolchain. Semiihosting is usually blocking and will affect code timing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change these settings in the board.h file for your LPCOpen release. You will need to rebuild the board library and example code after making the change.&lt;/P&gt;&lt;H3 id="toc-hId--1849680284"&gt;&lt;/H3&gt;&lt;H3 id="toc-hId--106869949"&gt;Additional information on setting up semihosting&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you setup the DEBUG* support for semihosting, you may need to also configure the toolchain to support semihosting. See the topic(s) below for more information on toolchain specific semihosting setup support.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/389153" rel="nofollow noopener noreferrer" target="_blank"&gt;LPCXPresso semihosting library support&lt;/A&gt;​&lt;/P&gt;&lt;H2 id="toc-hId-1832453891"&gt;&lt;/H2&gt;&lt;H2 id="toc-hId--719703070"&gt;&lt;SPAN style="color: #eb7a3d;"&gt;DEBUGINIT()&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;STRONG&gt;DEBUGINIT&lt;/STRONG&gt;() function definition sets up the debug input and output device(s). This needs to be called prior to calling any other DEBUG* functions. If DEBUG_ENABLE is not defined, this function will do nothing. If DEBUG_ENABLE is defined, but DEBUG_SEMIHOSTING is not defined, then the default LPCOpen implementation will attempt to use a UART for debug input and output. For most LPCOpen platforms, these functions are already setup to the available UART interface for the board. You can change the functions to another implementation if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For all LPCOpen release, the &lt;STRONG&gt;DEBUGINIT&lt;/STRONG&gt;() function is called automatically when you called Board_Init(). If you don't use a board layer in your example, but use these functions, you will need to call &lt;STRONG&gt;DEBUGINIT&lt;/STRONG&gt;() in your code.&lt;/P&gt;&lt;H2 id="toc-hId-1023107265"&gt;&lt;/H2&gt;&lt;H2 id="toc-hId--1529049696"&gt;&lt;SPAN style="color: #eb7a3d;"&gt;DEBUGOUT()&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;STRONG&gt;DEBUGOUT&lt;/STRONG&gt;() function provides formatted output to the debug output device. This maps to the printf() function whenever DEBUG_ENABLE is defined. The formatted string must be null terminated.&lt;/P&gt;&lt;H2 id="toc-hId-213760639"&gt;&lt;/H2&gt;&lt;H2 id="toc-hId--1453119757"&gt;&lt;SPAN style="color: #eb7a3d;"&gt;DEBUGSTR()&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;STRONG&gt;DEBUGSTR&lt;/STRONG&gt;() function simply outputs a raw string to the debug output device when DEBUG_ENABLE is defined. If DEBUG_SEMIHOSTING is defined, this maps to the printf() function. If DEBUG_SEMIHOSTING is not defined, then the raw string data is routed out top the output device directly. When not using semihosting, using this implementation over &lt;STRONG&gt;DEBUGOUT&lt;/STRONG&gt;() can save memory since the formatting library isn't needed. The string or data must be null terminated.&lt;/P&gt;&lt;H2 id="toc-hId-289690578"&gt;&lt;/H2&gt;&lt;H2 id="toc-hId-2032500913"&gt;&lt;SPAN style="color: #eb7a3d;"&gt;DEBUGIN()&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;STRONG&gt;DEBUGIN&lt;/STRONG&gt;() function is used to poll the debug input device for a character. This function never blocks and will always return a single character value or EOF. If DEBUG_ENABLE is not defined, or both DEBUG_ENABLE and DEBUG_SEMIHOSTING are defined, then this function will return EOF. If DEBUG_ENABLE is defined and DEBUG_SEMIHOSTING is not defined, then the function will return a singel byte read from the device if it exists or EOF if no data exists.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 15:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471314#M114</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-22T15:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen debug input/output support</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471315#M115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="submitted"&gt;&lt;SPAN class="comment-id"&gt;#1&lt;/SPAN&gt;Submitted by nicolasberan on Tue, 2014-07-08 22:16.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi, im trying yo change the DEBUGIN() macro, i need to use getchar so i replaced the DEBUGIN() Board_UARTGetChar() with the getchar() but when i do it, the macro seem like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(--(((&amp;amp;__Ciob[0]))-&amp;gt;__icnt) &amp;gt;= 0 ? *(((&amp;amp;__Ciob[0]))-&amp;gt;__ptr)++ : __filbuf((&amp;amp;__Ciob[0])))&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i replace the DEBUGIN() instruction with getchar(), it works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 16:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471315#M115</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-22T16:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen debug input/output support</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471316#M116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="comment-id"&gt;#2&lt;/SPAN&gt;Submitted by hetii on Tue, 2014-06-10 03:32.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same here... &lt;BR /&gt; Please advise.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 16:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471316#M116</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-22T16:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen debug input/output support</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471317#M117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="submitted"&gt;&lt;SPAN class="comment-id"&gt;#3&lt;/SPAN&gt;Submitted by pat-will on Sat, 2014-05-10 07:37.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also not working for me. It seems that there is nothing happening even if i just call printf. I even tried a fresh install following these instructions but no luck. I am using the LPC 1769, Rev C on a microsoft computer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 16:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471317#M117</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-22T16:14:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen debug input/output support</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471318#M118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="comment-id"&gt;#4&lt;/SPAN&gt;Submitted by Palesky on Sat, 2014-04-26 02:56.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems not to work properly.&lt;BR /&gt; I downloaded the following file and imported it into LPCXpresso v7.1.1_125.&lt;BR /&gt; lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip&lt;BR /&gt; Then I modified board.h to define DEBUG_ENABLE and DEBUG_SEMIHOSTING. But DEBUGOUT does not print anything to console at all.&lt;BR /&gt; I tried it with "webserver" project and "lwip_tcpecho_sa" project.&lt;BR /&gt; Is what I did wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 16:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471318#M118</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-22T16:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen debug input/output support</title>
      <link>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471319#M119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="submitted"&gt;&lt;SPAN class="comment-id"&gt;#5&lt;/SPAN&gt;Submitted by hetii on Fri, 2014-11-14 03:47.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi there&lt;/P&gt;&lt;P&gt;I discovered that you need to add "\r\n" at the end of each string for DEBUG* functions, otherwise IDE simply ignore it.&lt;BR /&gt; Eg: DEBUGSTR("Hello!\r\n"); instead DEBUGSTR("Hello!");&lt;/P&gt;&lt;P&gt;Also keep in mind that "semihosting" functionality must be enabled:&lt;BR /&gt; Eg: Project -&amp;gt; Properties -&amp;gt; C/C++ Build -&amp;gt; Settings -&amp;gt; Tool Settings(first tab) -&amp;gt; MCU Linker -&amp;gt; Manager Linker Script -&amp;gt; Library -&amp;gt; Redlib(semihosting)&lt;/P&gt;&lt;P&gt;Additional useful information can be found here: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/389140"&gt;Using printf()&lt;/A&gt;​&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 16:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-FAQs/LPCOpen-debug-input-output-support/m-p/471319#M119</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-22T16:22:16Z</dc:date>
    </item>
  </channel>
</rss>