<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPCOpen and USART in synchronous mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-and-USART-in-synchronous-mode/m-p/513288#M99</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cosborne2000 on Sat Jun 21 09:16:33 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to use the USART in synchronous mode and I'm trying to stick with the LPCOpen framework.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The synchronous bits are included in the macros but don't appear to be referenced in the functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use the LPCOpen functions for USART synchronous mode? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;note: both SPI functions are already in use.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:05:13 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:05:13Z</dc:date>
    <item>
      <title>LPCOpen and USART in synchronous mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-and-USART-in-synchronous-mode/m-p/513288#M99</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cosborne2000 on Sat Jun 21 09:16:33 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to use the USART in synchronous mode and I'm trying to stick with the LPCOpen framework.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The synchronous bits are included in the macros but don't appear to be referenced in the functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use the LPCOpen functions for USART synchronous mode? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;note: both SPI functions are already in use.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-and-USART-in-synchronous-mode/m-p/513288#M99</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen and USART in synchronous mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-and-USART-in-synchronous-mode/m-p/513289#M100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cosborne2000 on Mon Jun 23 07:55:15 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've never used the USART in synchronous mode before so I must be missing something basic.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Communication with device is OK with SPI module (SPI1 mode 1 master).&amp;nbsp; When I switch to USART1 in sync mode I get nothing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't have access to my scope this week so I can't check the waveforms to confirm the signals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Basic questions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. can USART work as a standard SPI mode 1 interface?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. I assumed that the start and stop bits were not sent in sync mode- is that correct?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. if I transmit an 8 bit frame in as master, is the RX register now holding 8 bits clocked in during the transmit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4. is there a basic example available demonstrating the USART in sync mode?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-and-USART-in-synchronous-mode/m-p/513289#M100</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:05:14Z</dc:date>
    </item>
  </channel>
</rss>