<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iType font converstion in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/iType-font-converstion/m-p/515044#M986</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Mon Jun 17 16:44:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Received word from Segger that this feature is only available with emFile installed...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:15:29 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:15:29Z</dc:date>
    <item>
      <title>iType font converstion</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/iType-font-converstion/m-p/515043#M985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Wed Jun 12 13:55:10 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I am using emWin 5.20.&amp;nbsp; As part of emWin5.20, the iType font generator is included as an option.&amp;nbsp; In linking in the source code, it is also trying to link in the header file "fs_api.h", which does not exist.&amp;nbsp; It appears, however, that this file is included with Segger's emFile system, which is not included as part of emWin's LCD license.&amp;nbsp; This begs the question... can we use iType on LPC's implementation of emWin?&amp;nbsp; If so, where is this file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/iType-font-converstion/m-p/515043#M985</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: iType font converstion</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/iType-font-converstion/m-p/515044#M986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Mon Jun 17 16:44:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Received word from Segger that this feature is only available with emFile installed...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/iType-font-converstion/m-p/515044#M986</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:15:29Z</dc:date>
    </item>
  </channel>
</rss>