<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: simple SPIFI setup for just reading data</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529706#M9851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Mon Aug 11 16:49:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Dill,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When you use LPC1837 you have both options. You can boot from SPIFI (jumper setting) or internal flash. You can mix code between internal flash and external QSPI/DSPI/SPI serial flash. You just need to place code/function in the serial flash. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:16:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:16:57Z</dc:date>
    <item>
      <title>simple SPIFI setup for just reading data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529705#M9850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dill on Mon Aug 11 13:53:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I used a flashless 1830 running from SPIFI but now I switched to a 1837 with internal flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With the 1830 the SPIFI just works, it behaves just like internal flash. I did not set any registers or call any init functions. Seems like there is going on some magic when the 1830 boots from spifi...?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, now that I'm booting from the internal flash it seems like I have to set up the SPIFI manually. How is this done? I only find help for booting/running code from SPIFI or *writing* to SPIFI (I just want to put a big array there using the prommer and READ it). Any pointers?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any decent info about SPIFI? The chapter in the user manual is just two pages and does not help at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for any help,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sebatian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:16:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529705#M9850</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:16:56Z</dc:date>
    </item>
    <item>
      <title>Re: simple SPIFI setup for just reading data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529706#M9851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Mon Aug 11 16:49:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Dill,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When you use LPC1837 you have both options. You can boot from SPIFI (jumper setting) or internal flash. You can mix code between internal flash and external QSPI/DSPI/SPI serial flash. You just need to place code/function in the serial flash. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529706#M9851</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: simple SPIFI setup for just reading data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529707#M9852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue Aug 12 00:40:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Dill&lt;/STRONG&gt;&lt;BR /&gt;The chapter in the user manual is just two pages&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the latest version it has 12 pages.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:16:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529707#M9852</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:16:58Z</dc:date>
    </item>
    <item>
      <title>Re: simple SPIFI setup for just reading data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529708#M9853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dill on Tue Aug 12 01:07:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt; You can boot from SPIFI (jumper setting)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't want to do this right now, but maybe later. Is this correct:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; - pull P2_7 down OR have no valid code in internal flash&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; - set boot pins to 1 OR set OTP/BOOT_SRC=3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I do this the 1837 will behave just like the flashless part does by default?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;While looking in the new (thanks!) UM right now, I now found something: 4.3.5.4 SPIFI boot mode:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The config seems to be done while booting&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; - "Setup Pin Configuration"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; - activate Vendor ID specific driver&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is why I do not have to do any config with the flashless part....?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So when NOT booting from SPIFI, I have to use the SPIFI lib and follow the steps in "LPCSPIFILIB library use model", am I right?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or is there an easier way? Like, just tell the UC to do the setup, but to NOT boot from SPIFI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks for your help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:16:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/simple-SPIFI-setup-for-just-reading-data/m-p/529708#M9853</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:16:59Z</dc:date>
    </item>
  </channel>
</rss>