<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Anyone using the LPC-Link 2 with MCB1857 KEIL development board?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529446#M9810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 11 12:46:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;How are you powering your MCB1857 board? I certainly wouldn't recommend powering from the LPC-Link2, if that is what you are doing. i.e. ensure that JP2 is not jumpered. Only use LPC-Link2 to power small/simple boards with minimal power requirements; certainly don't use it to power complex boards with LCDs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:17:37 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:17:37Z</dc:date>
    <item>
      <title>Anyone using the LPC-Link 2 with MCB1857 KEIL development board?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529445#M9809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jstoner on Mon Aug 11 09:37:47 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I Have had inductor L3 burn on two LPC-Link 2 boards while connected for debug to a KEIL MCB1857 development board.&amp;nbsp; It will happen at a seemingly random time while the debugger is connected.&amp;nbsp; Everything works fine until that point.&amp;nbsp; Has anyone else using this configuration had the same problem or other issues?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529445#M9809</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone using the LPC-Link 2 with MCB1857 KEIL development board?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529446#M9810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 11 12:46:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;How are you powering your MCB1857 board? I certainly wouldn't recommend powering from the LPC-Link2, if that is what you are doing. i.e. ensure that JP2 is not jumpered. Only use LPC-Link2 to power small/simple boards with minimal power requirements; certainly don't use it to power complex boards with LCDs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:17:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529446#M9810</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:17:37Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone using the LPC-Link 2 with MCB1857 KEIL development board?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529447#M9811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jstoner on Mon Aug 11 15:54:28 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the response.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When the failure occured it was being powered by two independent USB cables (one for the LPC-Link2 and one for the MCB1857).&amp;nbsp; I'm certain JP2 was not installed on the most recent failure, but I am not sure about the first one.&amp;nbsp; We have been using the LPC-Link2 with no problems on a smaller dev board (in JP2 and non-JP2 configurations). We will make sure going forward that no one is installing JP2 while connected to the MCB1857.&amp;nbsp; We'll keep an eye on it and see if it happens again.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Anyone-using-the-LPC-Link-2-with-MCB1857-KEIL-development-board/m-p/529447#M9811</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:17:38Z</dc:date>
    </item>
  </channel>
</rss>