<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: 16-color, 4bpp using custom palette under emwin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515015#M975</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Tue Apr 23 17:54:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;/P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:16:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:16:23Z</dc:date>
    <item>
      <title>16-color, 4bpp using custom palette under emwin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515012#M972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Fri Apr 19 16:45:04 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I am intending on running emWin using built in RAM only.&amp;nbsp; I do not want to use more than half of the built in RAM for display buffering, and our application allows us to run the display using a fixed, custom 16-color palette (which can be themed) using 4bpp mappings.&amp;nbsp; This would utilize roughly 35K of RAM for a 320x240 LCD.&amp;nbsp; Is there an example of the code required to set this up?&amp;nbsp; I am pretty sure the LPC1788 supports this mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:16:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515012#M972</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:16:21Z</dc:date>
    </item>
    <item>
      <title>Re: 16-color, 4bpp using custom palette under emwin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515013#M973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Mon Apr 22 04:46:08 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;The LCP1788 LCD controller is very easy to set up. Just look in the manual and setup the register.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;But: if you want to change the display contents without visible screen disturbance, you have to use 2 RAM buffers. So I think your approch of using only internal RAM will not work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515013#M973</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:16:22Z</dc:date>
    </item>
    <item>
      <title>Re: 16-color, 4bpp using custom palette under emwin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515014#M974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Tue Apr 23 17:54:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I was hoping to avoid having to write a from-scratch c-program, and leverage emwin for this application.&amp;nbsp; What I could not determine from the emWin documentation is how to establish a custom pallete to work with a 4bpp drive.&amp;nbsp; I think its about initializing emWin properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515014#M974</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:16:22Z</dc:date>
    </item>
    <item>
      <title>Re: 16-color, 4bpp using custom palette under emwin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515015#M975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Tue Apr 23 17:54:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;/P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/16-color-4bpp-using-custom-palette-under-emwin/m-p/515015#M975</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:16:23Z</dc:date>
    </item>
  </channel>
</rss>