<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックprogram that is loaded by secondary bootloader UART handler doesn't return</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/program-that-is-loaded-by-secondary-bootloader-UART-handler/m-p/528526#M9632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by internav on Fri Jan 31 15:21:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the secondary bootloader to load a program and when the program executes and the uart interrupt handler is entered, it returns to neverland.&amp;nbsp; The systick and timer handlers work fine.&amp;nbsp; the bootloader uses the uart but polls for data and uses no interrupts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the bootloader is in flash from 0-0x1fff and the program starts at 0x2000. The test program sits in a while loop and has only systick and uart handlers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;if I take the test program and build at location 0 and run, it works fine.&amp;nbsp; and the assembly code looks the same for both versions.&amp;nbsp; so it has to be some complier linker setting?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;attached are the zips for the bootloader and test boot program.&lt;/SPAN&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338028"&gt;bootloader.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338028"&gt;boot_test.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:29:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:29:06Z</dc:date>
    <item>
      <title>program that is loaded by secondary bootloader UART handler doesn't return</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/program-that-is-loaded-by-secondary-bootloader-UART-handler/m-p/528526#M9632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by internav on Fri Jan 31 15:21:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the secondary bootloader to load a program and when the program executes and the uart interrupt handler is entered, it returns to neverland.&amp;nbsp; The systick and timer handlers work fine.&amp;nbsp; the bootloader uses the uart but polls for data and uses no interrupts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the bootloader is in flash from 0-0x1fff and the program starts at 0x2000. The test program sits in a while loop and has only systick and uart handlers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;if I take the test program and build at location 0 and run, it works fine.&amp;nbsp; and the assembly code looks the same for both versions.&amp;nbsp; so it has to be some complier linker setting?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;attached are the zips for the bootloader and test boot program.&lt;/SPAN&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338028"&gt;bootloader.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338028"&gt;boot_test.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/program-that-is-loaded-by-secondary-bootloader-UART-handler/m-p/528526#M9632</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: program that is loaded by secondary bootloader UART handler doesn't return</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/program-that-is-loaded-by-secondary-bootloader-UART-handler/m-p/528527#M9633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Champion on Mon Apr 28 20:43:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi internav,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"if I take the test program and build at location 0 and run, it works fine. " &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the same problem.&amp;nbsp; Did you find a solution?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/program-that-is-loaded-by-secondary-bootloader-UART-handler/m-p/528527#M9633</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:29:07Z</dc:date>
    </item>
  </channel>
</rss>