<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Calling USB ROM API functions from internal SRAM raise Hard Fault exception in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Calling-USB-ROM-API-functions-from-internal-SRAM-raise-Hard/m-p/528472#M9618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Harvester on Wed Oct 07 14:17:41 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to write the code used USB ROM API functions, which will be executed from internal SRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had try to run some usbd_rom examples (ie, cdc_vcom) from internal SRAM. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had define new Target, set IROM1: 0x10000000...0x10008000 and IRAM2: 0x20000000...0x20010000, select "lpc18xx_43xx_debug_iram.ini" initialization file. An application starts but durin executing USBD_API-&amp;gt;hw-&amp;gt;Init() function Hard Fault exception is rised .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What I must do to solve this problem?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:16:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:16:50Z</dc:date>
    <item>
      <title>Calling USB ROM API functions from internal SRAM raise Hard Fault exception</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Calling-USB-ROM-API-functions-from-internal-SRAM-raise-Hard/m-p/528472#M9618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Harvester on Wed Oct 07 14:17:41 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to write the code used USB ROM API functions, which will be executed from internal SRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had try to run some usbd_rom examples (ie, cdc_vcom) from internal SRAM. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had define new Target, set IROM1: 0x10000000...0x10008000 and IRAM2: 0x20000000...0x20010000, select "lpc18xx_43xx_debug_iram.ini" initialization file. An application starts but durin executing USBD_API-&amp;gt;hw-&amp;gt;Init() function Hard Fault exception is rised .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What I must do to solve this problem?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Calling-USB-ROM-API-functions-from-internal-SRAM-raise-Hard/m-p/528472#M9618</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: Calling USB ROM API functions from internal SRAM raise Hard Fault exception</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Calling-USB-ROM-API-functions-from-internal-SRAM-raise-Hard/m-p/528473#M9619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Harvester on Fri Oct 09 02:23:57 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm sorry, it's my mistake. I didn't change base address for USB stack buffer (0x200000000).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Calling-USB-ROM-API-functions-from-internal-SRAM-raise-Hard/m-p/528473#M9619</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:16:51Z</dc:date>
    </item>
  </channel>
</rss>