<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC1768nxpUSBLib v0.98 to communication over USB cable (CDC)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527386#M9385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which LPC board are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, Have you tried to use another VCOM terminal such as Teraterm or Putty? or were you able to capture the USB transactions with an USB sniffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 22:28:24 GMT</pubDate>
    <dc:creator>isaacavila</dc:creator>
    <dc:date>2016-07-28T22:28:24Z</dc:date>
    <item>
      <title>LPC1768nxpUSBLib v0.98 to communication over USB cable (CDC)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527385#M9384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a LPC1768 and I am using nxpUSBLib v0.98 to communicate over USB cable (CDC). LPC (Device) to PC (Host). I have used the example virtualCOM. When I connect my device in my computer and the port COM is Ok. But I can't communicate with the device using pipocom. I my host sends URB_BULK&amp;nbsp; out, but my device (LPC) doesn't recive this information. Do you know what can be?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2016 14:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527385#M9384</guid>
      <dc:creator>thiagosiqueira</dc:creator>
      <dc:date>2016-07-01T14:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768nxpUSBLib v0.98 to communication over USB cable (CDC)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527386#M9385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which LPC board are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, Have you tried to use another VCOM terminal such as Teraterm or Putty? or were you able to capture the USB transactions with an USB sniffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 22:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527386#M9385</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-07-28T22:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768nxpUSBLib v0.98 to communication over USB cable (CDC)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527387#M9386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Isaac. The problem was my interrupt function that wasn't correct. The library and the example works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 13:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768nxpUSBLib-v0-98-to-communication-over-USB-cable-CDC/m-p/527387#M9386</guid>
      <dc:creator>thiagosiqueira</dc:creator>
      <dc:date>2016-12-27T13:40:55Z</dc:date>
    </item>
  </channel>
</rss>