<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC15xx USB-less ISP</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526505#M9135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EtaPhi on Thu Aug 21 05:41:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;starblue, LabRat, your replies are very helpful for me that I'm discovering LPC micros.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My initial development is going to use a LPCXpresso LPC1549 board, while the first prototype board is being built, so USB isn't a real issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's however an issue for the final application, which is airborne.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Since it's a scientific mission, there is no need to comply with DO-179 regulations, but it's better to agree with their mindset, which may be summoned as: "what doesn't exist, can't broke!".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;USB support adds weight and pcb space due to connector, ESD protection devices, etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's almost useless for my application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If there exists a part without USB (as it exists), I prefer it, because I don't have to provide evidence that a bug my activate that unused feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Even if LPC15xx micros are COTS (commercial off-the-shelf) components, a triple redundant system, i.e. three LPC15xx working in parallel, with an appropriate voting logic should be DO-179 compliant (if submitted to a third-party certifying authority).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Airborne devices may experience unexpected resets, which may be due to ionizing particles, EMI etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's therefore better to recover from such events as quick as possible, but ISP bootloader must not interfere with reboots.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is the reason of my request, which addresses a documentation void.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EtaPhi&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:04:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:04:43Z</dc:date>
    <item>
      <title>LPC15xx USB-less ISP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526502#M9132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EtaPhi on Thu Aug 21 00:54:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm new to NXP microcontroller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm developing a board to control a PMSM with FOC algoritm.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My board is going to use a LPC1519JBD64 or LPC1518JDB64 or LPC1517JBD64 according to the computing resources that my final firmware will need.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I wonder what may happen when ISP_0 (PIO1_9) and ISP_1 (PIO1_11) are both pulled up and my firmware signature isn't valid.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC15xx datasheet says that in such case, the USB bootloader is run, but these parts have no USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Should I provide my board with dip-switches to select USART0 ISP mode (or C_CAN mode) as a safety measure?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll really appreciate any suggestion.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EtaPhi&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526502#M9132</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC15xx USB-less ISP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526503#M9133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Thu Aug 21 02:26:16 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Without USB you probably shouldn't pull up ISP_0 and ISP_1 in the first place. Rather pull down ISP_0 and use ISP_1 to select between CAN and UART (if necessary, otherwise just pull it low/high).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Jürgen&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526503#M9133</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC15xx USB-less ISP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526504#M9134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LabRat on Thu Aug 21 02:35:51 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: EtaPhi&lt;/STRONG&gt;&lt;BR /&gt;Should I provide my board with dip-switches to select USART0 ISP mode (or C_CAN mode) as a safety measure?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's helpful to add jumpers to pull down ISP0/1 (to switch to UART) and a pin header (UART0 RXD / UART0 TXD / GND) to connect an UART to USB converter&amp;nbsp; :) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If SWD is failing (or you are flashing an image which is deactivating SWD...) you can use FlashMagic to erase the chip...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course you can also use C_CAN (if you add a CAN transceiver), but there's no free Software / Tool to use C_CAN bootloader.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Since USB can be added very easy to your board, it could also be a good idea to use a 1549 during development... &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526504#M9134</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC15xx USB-less ISP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526505#M9135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EtaPhi on Thu Aug 21 05:41:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;starblue, LabRat, your replies are very helpful for me that I'm discovering LPC micros.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My initial development is going to use a LPCXpresso LPC1549 board, while the first prototype board is being built, so USB isn't a real issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's however an issue for the final application, which is airborne.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Since it's a scientific mission, there is no need to comply with DO-179 regulations, but it's better to agree with their mindset, which may be summoned as: "what doesn't exist, can't broke!".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;USB support adds weight and pcb space due to connector, ESD protection devices, etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's almost useless for my application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If there exists a part without USB (as it exists), I prefer it, because I don't have to provide evidence that a bug my activate that unused feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Even if LPC15xx micros are COTS (commercial off-the-shelf) components, a triple redundant system, i.e. three LPC15xx working in parallel, with an appropriate voting logic should be DO-179 compliant (if submitted to a third-party certifying authority).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Airborne devices may experience unexpected resets, which may be due to ionizing particles, EMI etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's therefore better to recover from such events as quick as possible, but ISP bootloader must not interfere with reboots.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is the reason of my request, which addresses a documentation void.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EtaPhi&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-USB-less-ISP/m-p/526505#M9135</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:04:43Z</dc:date>
    </item>
  </channel>
</rss>