<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1227 GPIO current consumption in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1227-GPIO-current-consumption/m-p/526454#M9084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alubeiro on Thu Dec 04 07:40:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi guys,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working with a LPC1227 which i enter in deep sleep mode. The issu appears when i want to keep GPIO0_20 as an output to high. In this case the current consumption is around 2.1mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the other hand when i put this pin to LOW, the current consumpion is around 30uA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This pin goes to nowhere cause i have lifted it up from the PCB, so it is astonishing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help will be apreciated. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and best regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alberto&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:02:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:02:42Z</dc:date>
    <item>
      <title>LPC1227 GPIO current consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1227-GPIO-current-consumption/m-p/526454#M9084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alubeiro on Thu Dec 04 07:40:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi guys,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working with a LPC1227 which i enter in deep sleep mode. The issu appears when i want to keep GPIO0_20 as an output to high. In this case the current consumption is around 2.1mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the other hand when i put this pin to LOW, the current consumpion is around 30uA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This pin goes to nowhere cause i have lifted it up from the PCB, so it is astonishing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help will be apreciated. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and best regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alberto&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1227-GPIO-current-consumption/m-p/526454#M9084</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1227 GPIO current consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1227-GPIO-current-consumption/m-p/526455#M9085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alubeiro on Tue Dec 09 01:20:05 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also realised that this issue happens with all GPIOs which can work as input comparators.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is anything special with this GPIOs that i have to do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help will be apreciated&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1227-GPIO-current-consumption/m-p/526455#M9085</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:02:43Z</dc:date>
    </item>
  </channel>
</rss>