<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Can WWDt can be used as regular timer lpc1317</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-WWDt-can-be-used-as-regular-timer-lpc1317/m-p/525869#M8505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usb10185 on Mon Aug 12 07:57:51 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes this is possible. Just use the Debug mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the Watchdog Mode register (WDMOD - address 0x4000 4000), set bits WDEN = 1 and WDRESET = 0 --&amp;gt; This is Watchdog interrupt mode: Debug with the Watchdog interrupt but no WDRESET enabled.When this mode is selected, a watchdog counter underflow will set the WDINT flag and the Watchdog interrupt request will be generated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ken&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:56:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:56:47Z</dc:date>
    <item>
      <title>Can WWDt can be used as regular timer lpc1317</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-WWDt-can-be-used-as-regular-timer-lpc1317/m-p/525868#M8504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aamir ali on Sun Aug 11 22:24:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;WWDT is used for counting for specified time &amp;amp; after that it reset the MCU. if its not kicked again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But can it be used as regular timer&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-WWDt-can-be-used-as-regular-timer-lpc1317/m-p/525868#M8504</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can WWDt can be used as regular timer lpc1317</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-WWDt-can-be-used-as-regular-timer-lpc1317/m-p/525869#M8505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usb10185 on Mon Aug 12 07:57:51 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes this is possible. Just use the Debug mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the Watchdog Mode register (WDMOD - address 0x4000 4000), set bits WDEN = 1 and WDRESET = 0 --&amp;gt; This is Watchdog interrupt mode: Debug with the Watchdog interrupt but no WDRESET enabled.When this mode is selected, a watchdog counter underflow will set the WDINT flag and the Watchdog interrupt request will be generated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ken&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-WWDt-can-be-used-as-regular-timer-lpc1317/m-p/525869#M8505</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:56:47Z</dc:date>
    </item>
  </channel>
</rss>