<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Problems getting the project to initialize</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514732#M850</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Wed Jun 05 17:49:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I have a version running on the EA LPC1788 platform, with Free Rtos.&amp;nbsp; I cannot get past the function call &amp;nbsp; GUI_ALLOC_AssignMemory(_aMemory, GUI_NUMBYTES), without it going into a while loop in GUI_Error called from _InitOnce (according to the Assembly Routine).&amp;nbsp; I have absolutely no insight as to what is broken.&amp;nbsp; The .GUI and .VRAM address spaces are all compiled and allocated correctly, and I successfully tested the SDRAM by writing and reading from the SDRAM location.&amp;nbsp; The code itself is called before the scheduler in FreeRtos as well, so as to eliminate that as a problem.&amp;nbsp; The LCDConf, GUIConf and most of the other files were merged into the main load from a working platform.&amp;nbsp; I have even verified that these are mostly identical to the originals.&amp;nbsp; Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:14:45 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:14:45Z</dc:date>
    <item>
      <title>Problems getting the project to initialize</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514732#M850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Wed Jun 05 17:49:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I have a version running on the EA LPC1788 platform, with Free Rtos.&amp;nbsp; I cannot get past the function call &amp;nbsp; GUI_ALLOC_AssignMemory(_aMemory, GUI_NUMBYTES), without it going into a while loop in GUI_Error called from _InitOnce (according to the Assembly Routine).&amp;nbsp; I have absolutely no insight as to what is broken.&amp;nbsp; The .GUI and .VRAM address spaces are all compiled and allocated correctly, and I successfully tested the SDRAM by writing and reading from the SDRAM location.&amp;nbsp; The code itself is called before the scheduler in FreeRtos as well, so as to eliminate that as a problem.&amp;nbsp; The LCDConf, GUIConf and most of the other files were merged into the main load from a working platform.&amp;nbsp; I have even verified that these are mostly identical to the originals.&amp;nbsp; Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514732#M850</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: Problems getting the project to initialize</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514733#M851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Wed Jun 05 18:25:06 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Never mind... I found the problem...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514733#M851</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: Problems getting the project to initialize</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514734#M852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wendtr on Wed Jun 05 18:26:12 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I found the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-getting-the-project-to-initialize/m-p/514734#M852</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:14:46Z</dc:date>
    </item>
  </channel>
</rss>