<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピック LPC1347 HID_SetReport and HID_GetReport functions NOT called</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1347-HID-SetReport-and-HID-GetReport-functions-NOT-called/m-p/525846#M8482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bonitusb on Wed Jun 25 19:03:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everyone, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;has anyone had success with the Lpc1347 USB_HID_Generic using IAR Embedded workbench?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I used Visual Basic to create my interface panel and it is working very fine with Lpc1343.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i am using this example bundle, "lpcopen_2_05_keil_iar_nxp_lpcxpresso_1347"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With LPC1347, i can connect the device to the host but the problem is that no information is exchanged between them. I also discovered that the two functions responsible for information exchange are not being called, i.e HID_SetReport and HID_GetReport. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone an idea?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:55:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:55:59Z</dc:date>
    <item>
      <title>LPC1347 HID_SetReport and HID_GetReport functions NOT called</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1347-HID-SetReport-and-HID-GetReport-functions-NOT-called/m-p/525846#M8482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bonitusb on Wed Jun 25 19:03:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everyone, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;has anyone had success with the Lpc1347 USB_HID_Generic using IAR Embedded workbench?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I used Visual Basic to create my interface panel and it is working very fine with Lpc1343.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i am using this example bundle, "lpcopen_2_05_keil_iar_nxp_lpcxpresso_1347"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With LPC1347, i can connect the device to the host but the problem is that no information is exchanged between them. I also discovered that the two functions responsible for information exchange are not being called, i.e HID_SetReport and HID_GetReport. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone an idea?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1347-HID-SetReport-and-HID-GetReport-functions-NOT-called/m-p/525846#M8482</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:59Z</dc:date>
    </item>
  </channel>
</rss>