<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 DFU supported with LPC1857 And IAP Command Code 57 (Reinvoke ISP)?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DFU-supported-with-LPC1857-And-IAP-Command-Code-57-Reinvoke-ISP/m-p/525668#M8304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by shansohn on Wed Dec 12 14:29:06 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an LPC1857 device that only supports firmware upgrade via USB0/DFU (hardwired per Table 13 of UM10430).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd like the application code to reinvoke ISP USB0/DFU on user command to upgrade firmware.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Q1: Can the Reinvoke ISP (IAP code 57) be used for this, or will that only support ISP via UART0?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Q2: If not, how would I reset the device so it enumerates back as a DFU-mode device. (e.g. invalidate the currently running flash bank so that ISP USB0/DFU mode will be run on the next device reset?)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:15:38 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:15:38Z</dc:date>
    <item>
      <title>DFU supported with LPC1857 And IAP Command Code 57 (Reinvoke ISP)?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DFU-supported-with-LPC1857-And-IAP-Command-Code-57-Reinvoke-ISP/m-p/525668#M8304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by shansohn on Wed Dec 12 14:29:06 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an LPC1857 device that only supports firmware upgrade via USB0/DFU (hardwired per Table 13 of UM10430).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd like the application code to reinvoke ISP USB0/DFU on user command to upgrade firmware.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Q1: Can the Reinvoke ISP (IAP code 57) be used for this, or will that only support ISP via UART0?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Q2: If not, how would I reset the device so it enumerates back as a DFU-mode device. (e.g. invalidate the currently running flash bank so that ISP USB0/DFU mode will be run on the next device reset?)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DFU-supported-with-LPC1857-And-IAP-Command-Code-57-Reinvoke-ISP/m-p/525668#M8304</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:15:38Z</dc:date>
    </item>
  </channel>
</rss>