<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Free Linux FLASH utility: mxli</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525552#M8188</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue Feb 11 01:48:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: MarcVonWindscooting&lt;/STRONG&gt;&lt;BR /&gt;I should set the default to 115200 if not lower. &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;115200 8N1 would be a nice default. If I remember correctly all the projects I worked on in recent years used that for their console.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;BTW, my test was on a Debian Linux.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:55:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:55:33Z</dc:date>
    <item>
      <title>Free Linux FLASH utility: mxli</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525549#M8185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MarcVonWindscooting on Thu Feb 06 16:01:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello Members,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was a bad boy!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I did not support LPC13xx with my Linux ISP flasher mxli until &lt;/SPAN&gt;&lt;STRONG&gt;today&lt;/STRONG&gt;&lt;SPAN&gt;, although I supported so many others.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;It can be found here: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.windscooting.com%2Fsofty%2Fmxli.html%23Latest" rel="nofollow" target="_blank"&gt;http://www.windscooting.com/softy/mxli.html#Latest&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Unfortunately, I've never used an LPC13xx so far. I count on you, providing some feedback!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And I would like to know if you consider this posting inappropriate for the LPCWare forum(s).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I started a PCB a few years ago, but then the project was canceled and two chips disappeared in the drawer. Later I used LPC1100 and LPC800. This is my first excuse, why support for a whole family kept missing from the program. The second excuse is: you could have programmed these chips with mxli anyway, from the first version on, just a little bit less comfortable. Only recently I found out, that people would rather modify the source code than provide a few command-line options. Pity, because that was one of the most important design requirements for mxli&amp;nbsp; :(( &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525549#M8185</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: Free Linux FLASH utility: mxli</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525550#M8186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Sat Feb 08 08:22:14 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Works for me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tested with a simple blinky on an Olimex LPC-P1343 board where I added a MAX3232 on the prototype area, and an FTDI-based USB-serial converter.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The default baud rate of 230400 was too high, 115200 worked.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe -x should be the default?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
$ ./mxli -b 115200 -x /home/juergen/git/jstlib/jstlib/targets/olimex_lpc-p1343/examples/blink-delay/build/outputs/olimex_lpc-p1343_blink-delay.hex
Detected: LPC1343, FLASH:32kiB, RAM0:8kiB, RAM1:0kiB, RAM2:0kiB
Image: 668 = 0x00029C Bytes
Transfer RAM: 7kiB+112B @ 0x10000270
Transmission RAM: 7blocks (7kiB), units of 1024B
Flash address range 0x00000000..0x000003ff, sectors: 0..0
Erasing sectors 0 to 0 NOW

Transfer block 0 to RAM (uuencode) ..OK.
Transfer block 0 to FLASH, sector 0 
Started program by system RESET
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525550#M8186</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: Free Linux FLASH utility: mxli</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525551#M8187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MarcVonWindscooting on Mon Feb 10 10:21:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your feedback!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, the baud rate is too high for most devices running from IRC, although that should not be a problem with a fractional divider.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm not sure if I never managed to use an USB-to-RS232 cable for the high rates, only devices that convert from USB to 3.3V-level RXD/TXD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I should set the default to 115200 if not lower. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Right now I'm still working on mxli, extending it to LPC43xx with dual bank FLASH. It turned out, the current version cannot flash a dual bank device, because it does not allow to define FLASH memory NOT starting at address 0. I missed that requirement :(&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And: mxli needs a detailed man-page with usage examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525551#M8187</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: Free Linux FLASH utility: mxli</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525552#M8188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue Feb 11 01:48:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: MarcVonWindscooting&lt;/STRONG&gt;&lt;BR /&gt;I should set the default to 115200 if not lower. &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;115200 8N1 would be a nice default. If I remember correctly all the projects I worked on in recent years used that for their console.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;BTW, my test was on a Debian Linux.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Free-Linux-FLASH-utility-mxli/m-p/525552#M8188</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:33Z</dc:date>
    </item>
  </channel>
</rss>