<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC conversion help in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525461#M8097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 06:25:24 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need some help figuring out why my ADC is not working properly.&amp;nbsp; I copied the code for the conversion from the periph_adc example.&amp;nbsp; My code is supposed to read from PIO0_11, divide the value by 50, and then output the value to 8 pins which are connected to LEDs and are functioning as my display using the little function I named "bytewriter".&amp;nbsp; I have verified that my 8 bit "display" is working properly.&amp;nbsp; I am using the LPC1347 board with usb. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; I am assuming that the board is providing the VREFN to VREFP/(V0 to Vdd) because the only power/ground pins on the board already have the correct voltage.&amp;nbsp; Is this an incorrect assumption?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The current behavior of my code is that it alternately displays values of 0 and 81 to my output pins.&amp;nbsp; 81 is 4095/50 so it seems to sometimes read high and sometimes read low.&amp;nbsp; Pin PIO0_11 is currently connected to 0.3V which is being supplied by a voltage regulator and resistor voltage divider.&amp;nbsp; I checked to make sure that this voltage was holding steady during operation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined (__USE_LPCOPEN)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined(NO_BOARD_LIB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "chip.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "board.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#include &amp;lt;cr_section_macros.h&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;// TODO: insert other include files here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;// TODO: insert other definitions and declarations here&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#ifdef __cplusplus&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;extern "C" {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#define _LPC_ADC_ID LPC_ADC&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;volatile uint32_t msTicks=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;static uint32_t rawTemp=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;static ADC_CLOCK_SETUP_T ADCSetup;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;// Systick Handler which is called each ms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void SysTick_Handler(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; msTicks++;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;// blocks for dlyTicks ms...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;static void Delay(uint32_t dlyTicks)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t curTicks;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; curTicks = msTicks;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while ((msTicks - curTicks) &amp;lt; dlyTicks);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;static void bytewriter(uint32_t bytevalue)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetPortMask(LPC_GPIO_PORT, 0, 0xFFFFFFF0);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetMaskedPortValue(LPC_GPIO_PORT, 0, bytevalue);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetPortMask(LPC_GPIO_PORT, 1, 0xFFFE1FFF);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bytevalue &amp;lt;&amp;lt;=9;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetMaskedPortValue(LPC_GPIO_PORT, 1, bytevalue);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;int main(void) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined (__USE_LPCOPEN)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if !defined(NO_BOARD_LIB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read clock settings and update SystemCoreClock variable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up and initialize all required blocks and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // functions related to the board hardware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_ADC_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the LED to the state of "On"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_LED_Set(0, true);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // TODO: insert code here&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Initialize Port GPIO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/color]Chip_GPIO_Init(LPC_GPIO_PORT);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_Init(_LPC_ADC_ID, &amp;amp;ADCSetup);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 0, (IOCON_FUNC1));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 1, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 2, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 3, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 13, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 14, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 15, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 16, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 11, (IOCON_FUNC2)|(IOCON_ADMODE_EN));&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Set Port 0 pins 0-3 and Port 1 pins 13-16 to output&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPortDIROutput(LPC_GPIO_PORT, 0, 0x0F);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPortDIROutput(LPC_GPIO_PORT, 1, 0x1E000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SysTick_Config(SystemCoreClock/1000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;while(1){&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Clear port bits&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_ClearValue(LPC_GPIO_PORT,0,0xF);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_ClearValue(LPC_GPIO_PORT,1,0x1E000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;uint16_t dataADC=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;rawTemp=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Read value from ADC Pin11&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;dataADC=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_EnableChannel(_LPC_ADC_ID, ADC_CH0, ENABLE);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_SetStartMode(_LPC_ADC_ID, ADC_START_NOW, ADC_TRIGGERMODE_RISING);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;while (Chip_ADC_ReadStatus(_LPC_ADC_ID, ADC_CH0, ADC_DR_DONE_STAT) != SET){}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_ReadValue(_LPC_ADC_ID, ADC_CH0, &amp;amp;dataADC);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Convert ADC data to value small enough to display on 8 bits&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;rawTemp = dataADC/50;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Set 8 bits to rawTemp value&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bytewriter(rawTemp);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Board_LED_Set(0, true);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Wait 1 second&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Delay(1000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Board_LED_Set(0, false);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//Wait 1 second&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Delay(1000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Force the counter to be placed into memory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile static int i = 0 ;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enter an infinite loop, just incrementing a counter&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i++ ;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0 ;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:54:22 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:54:22Z</dc:date>
    <item>
      <title>ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525461#M8097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 06:25:24 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need some help figuring out why my ADC is not working properly.&amp;nbsp; I copied the code for the conversion from the periph_adc example.&amp;nbsp; My code is supposed to read from PIO0_11, divide the value by 50, and then output the value to 8 pins which are connected to LEDs and are functioning as my display using the little function I named "bytewriter".&amp;nbsp; I have verified that my 8 bit "display" is working properly.&amp;nbsp; I am using the LPC1347 board with usb. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; I am assuming that the board is providing the VREFN to VREFP/(V0 to Vdd) because the only power/ground pins on the board already have the correct voltage.&amp;nbsp; Is this an incorrect assumption?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The current behavior of my code is that it alternately displays values of 0 and 81 to my output pins.&amp;nbsp; 81 is 4095/50 so it seems to sometimes read high and sometimes read low.&amp;nbsp; Pin PIO0_11 is currently connected to 0.3V which is being supplied by a voltage regulator and resistor voltage divider.&amp;nbsp; I checked to make sure that this voltage was holding steady during operation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined (__USE_LPCOPEN)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined(NO_BOARD_LIB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "chip.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "board.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#include &amp;lt;cr_section_macros.h&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;// TODO: insert other include files here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;// TODO: insert other definitions and declarations here&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#ifdef __cplusplus&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;extern "C" {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#define _LPC_ADC_ID LPC_ADC&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;volatile uint32_t msTicks=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;static uint32_t rawTemp=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;static ADC_CLOCK_SETUP_T ADCSetup;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;// Systick Handler which is called each ms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void SysTick_Handler(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; msTicks++;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;// blocks for dlyTicks ms...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;static void Delay(uint32_t dlyTicks)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t curTicks;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; curTicks = msTicks;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while ((msTicks - curTicks) &amp;lt; dlyTicks);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;static void bytewriter(uint32_t bytevalue)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetPortMask(LPC_GPIO_PORT, 0, 0xFFFFFFF0);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetMaskedPortValue(LPC_GPIO_PORT, 0, bytevalue);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetPortMask(LPC_GPIO_PORT, 1, 0xFFFE1FFF);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bytevalue &amp;lt;&amp;lt;=9;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_SetMaskedPortValue(LPC_GPIO_PORT, 1, bytevalue);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;int main(void) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined (__USE_LPCOPEN)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if !defined(NO_BOARD_LIB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read clock settings and update SystemCoreClock variable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up and initialize all required blocks and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // functions related to the board hardware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_ADC_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the LED to the state of "On"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_LED_Set(0, true);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // TODO: insert code here&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Initialize Port GPIO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/color]Chip_GPIO_Init(LPC_GPIO_PORT);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_Init(_LPC_ADC_ID, &amp;amp;ADCSetup);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 0, (IOCON_FUNC1));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 1, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 2, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 3, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 13, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 14, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 15, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 16, (IOCON_FUNC0));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 11, (IOCON_FUNC2)|(IOCON_ADMODE_EN));&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Set Port 0 pins 0-3 and Port 1 pins 13-16 to output&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPortDIROutput(LPC_GPIO_PORT, 0, 0x0F);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPortDIROutput(LPC_GPIO_PORT, 1, 0x1E000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SysTick_Config(SystemCoreClock/1000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;while(1){&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Clear port bits&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_ClearValue(LPC_GPIO_PORT,0,0xF);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_GPIO_ClearValue(LPC_GPIO_PORT,1,0x1E000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;uint16_t dataADC=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;rawTemp=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Read value from ADC Pin11&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;dataADC=0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_EnableChannel(_LPC_ADC_ID, ADC_CH0, ENABLE);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_SetStartMode(_LPC_ADC_ID, ADC_START_NOW, ADC_TRIGGERMODE_RISING);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;while (Chip_ADC_ReadStatus(_LPC_ADC_ID, ADC_CH0, ADC_DR_DONE_STAT) != SET){}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_ADC_ReadValue(_LPC_ADC_ID, ADC_CH0, &amp;amp;dataADC);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Convert ADC data to value small enough to display on 8 bits&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;rawTemp = dataADC/50;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Set 8 bits to rawTemp value&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bytewriter(rawTemp);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Board_LED_Set(0, true);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//Wait 1 second&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Delay(1000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Board_LED_Set(0, false);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//Wait 1 second&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Delay(1000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Force the counter to be placed into memory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile static int i = 0 ;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enter an infinite loop, just incrementing a counter&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i++ ;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0 ;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525461#M8097</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:22Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525462#M8098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue Mar 10 07:06:35 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;&lt;SPAN&gt;Quote: &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:cthvx8@hotmail.com"&gt;cthvx8@hotmail.com&lt;/A&gt;&lt;/STRONG&gt;&lt;BR /&gt;I am assuming that the board is providing the VREFN to VREFP/(V0 to Vdd)...&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :quest: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Which board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525462#M8098</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525463#M8099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 10:22:08 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;My board is OM13045.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525463#M8099</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525464#M8100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 10:23:27 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have not been able to find a schematic for the board.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525464#M8100</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525465#M8101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue Mar 10 11:05:44 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That's the LPC1347 LPCXpresso Board&amp;nbsp; :O &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Schematic:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.embeddedartists.com%2Fproducts%2Flpcxpresso%2Flpc1347_xpr.php" rel="nofollow" target="_blank"&gt;http://www.embeddedartists.com/products/lpcxpresso/lpc1347_xpr.php&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LQFP48 has no VREFP / VREFN pins, they are connected to VDD / VSS...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you try / debug the original adc example?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525465#M8101</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525466#M8102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 11:08:31 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No I did not yet.&amp;nbsp; I will try it.&amp;nbsp; Should ADC work properly while connected through the usb LPC link?&amp;nbsp; That is how I am currently powering the board.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525466#M8102</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525467#M8103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue Mar 10 11:12:18 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;&lt;SPAN&gt;Quote: &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:cthvx8@hotmail.com"&gt;cthvx8@hotmail.com&lt;/A&gt;&lt;/STRONG&gt;&lt;BR /&gt;No I did not yet.&amp;nbsp; I will try it.&amp;nbsp; Should ADC work properly while connected through the usb LPC link?&amp;nbsp; That is how I am currently powering the board.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, of course&amp;nbsp; :) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just add a simple voltage divider (2 x 10kOhm) to your ADC pin and try to measure VDD/2...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525467#M8103</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:27Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525468#M8104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 11:41:17 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ok, I tried periph_adc.&amp;nbsp; It is reading 0 sometimes, 4095 other times.&amp;nbsp; I confirmed the voltage is holding at 0.3 so it should be measuring around 372.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525468#M8104</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:27Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525469#M8105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue Mar 10 12:00:45 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;&lt;SPAN&gt;Quote: &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:cthvx8@hotmail.com"&gt;cthvx8@hotmail.com&lt;/A&gt;&lt;/STRONG&gt;&lt;BR /&gt;Ok, I tried periph_adc.&amp;nbsp; It is reading 0 sometimes, 4095 other times.&amp;nbsp; I confirmed the voltage is holding at 0.3 so it should be measuring around 372.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sample is working here without problems&amp;nbsp; :O &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Are you reading dataADC in App_Polling_Test() ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525469#M8105</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525470#M8106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cthvx8@hotmail.com on Tue Mar 10 14:03:58 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ok, I re-tried my exact same code using a higher voltage at the measurement point (~1.54) and it worked.&amp;nbsp; I added a resistor to bring the voltage down further (~1) and that worked too.&amp;nbsp; I will have to do some more experimentation but is there a known issue with measureing small voltages?&amp;nbsp; I was trying to measure 0.3V before.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-conversion-help/m-p/525470#M8106</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:54:29Z</dc:date>
    </item>
  </channel>
</rss>