<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC43xx - LPCUSBlib - MassStorageHost performance in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525231#M7867</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by AntonioL on Fri Mar 22 07:15:17 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thank you for your comments.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was aware that the payload data is wrapped with protocol data and divided in many packets, but really I didn' imagine how much.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried with a USB analyzer and effectively I found out that:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- with same USB flash key, just formatted and with the same single file (10MB payload) saved onto it&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- with a PC it reports an actual bandwidth usage of 128-130Mbps&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- with the MPC board it reports 115Mbps (and it takes 1.07s to tranfer the file - measured with an oscilloscope on a signalling pin)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Therefore the BW is almost the same.. I couldn't imagine the traffic was about 50% more than the payload transfer rate (115Mbps Vs 75Mbps).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Antonio&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:53:20 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:53:20Z</dc:date>
    <item>
      <title>LPC43xx - LPCUSBlib - MassStorageHost performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525229#M7865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by AntonioL on Tue Mar 19 04:59:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello to everybody&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am testing the performances of a LPC4357 (on a MCB4357 Keil dev board), USB port 0 HS as Mass Storage Host, using the LPCopen platform - LPCUSBlib dedicated example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anybody know how much can I expect? I bet not the theoretical 480Mbit/s, but I'd like to know how far one can go.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;At the moment I tried with different MSD flash disks and choose the fastest, then I tried to tune the buffer size (in MassStorageHost.c, static uint8_t buffer[8*1024];) also increasing its size (placing&amp;nbsp; it to the second portion of the ram through an explicit __attribute__((at(0x20000000))) ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I discovered that to read a 10MBytes file from the MSD, it takes about 1010ms with 8kB buffer, it increases significantly if I lower the size (2094ms with 2kB buffer), while rising it to 16-32 or even 64 kB doesn't improve very much (at minimun I get 994ms).. i.e I get approx 70-80Mbit/s rate at most.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it normal/the maximum I can achieve?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a look also at the LPCUSBlib and found in the LPCUSBlibConfig.h the USBRAM_BUFFER_SIZE define (default 4kB), but cannot increase it otherwise the linker won't find enough space.. is it related to the bandwidth limitation I am experiencing or is there something else to optimize?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Antonio&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525229#M7865</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx - LPCUSBlib - MassStorageHost performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525230#M7866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tuong on Wed Mar 20 03:31:25 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have you compared with your PC or other platforms? What is the result? Please try in following conditions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; - Same USB thumb drive&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; - Same read/write location (read/write on the begining of the drive always faster than on the end of the drive)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;FYI, 480Mbit/s is the USB high speed bit speed, you cannot calculate your expected time for 10MBytes file transfer from 480Mbits/s, as your file will not be transmitted continuously, it will be devided to many packets, each packet is wrapped by USB protocol data (SYNC,PID,ADD,your valid data,CRC) then transfered on USB bus.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With best regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525230#M7866</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx - LPCUSBlib - MassStorageHost performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525231#M7867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by AntonioL on Fri Mar 22 07:15:17 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thank you for your comments.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was aware that the payload data is wrapped with protocol data and divided in many packets, but really I didn' imagine how much.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried with a USB analyzer and effectively I found out that:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- with same USB flash key, just formatted and with the same single file (10MB payload) saved onto it&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- with a PC it reports an actual bandwidth usage of 128-130Mbps&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- with the MPC board it reports 115Mbps (and it takes 1.07s to tranfer the file - measured with an oscilloscope on a signalling pin)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Therefore the BW is almost the same.. I couldn't imagine the traffic was about 50% more than the payload transfer rate (115Mbps Vs 75Mbps).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Antonio&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525231#M7867</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:53:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx - LPCUSBlib - MassStorageHost performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525232#M7868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alexandermas on Sun Apr 20 00:53:15 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;To lift productivity it is necessary to increase the size of the buffer (PIPE_MAX_SIZE), to increase the FRAMELIST_SIZE_BITS size, to optimize the functions Pipe_Read_Stream_LE, Pipe_Write_Stream_LE at me in the project with freertos and lwip reading speed 10mb/s in a mode without wasps speed to 15-18mb/s at me PIPE_MAX_SIZE = 16кб, with double buffering, FRAMELIST_SIZE_BITS =5, the standard manager of memory is removed, instead of it another is used, by heap in sdram. cpu lpc4357 at 204mhz&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-LPCUSBlib-MassStorageHost-performance/m-p/525232#M7868</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:53:20Z</dc:date>
    </item>
  </channel>
</rss>