<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRequest: Example code for LPC11U2X/3X of CDC using USB rom'ed driver.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Request-Example-code-for-LPC11U2X-3X-of-CDC-using-USB-rom-ed/m-p/525212#M7848</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larsen on Mon Dec 10 03:19:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We are looking for examples for CDC class using the USB ROM'ed driver for LPC11U2X, LPC11U3X.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We thought it would be simpler to use the Rom'ed drivers than using the nxpUSBlib, but without good examples as a starting point this is not the case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any one with a pointer to some examples?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:52:21 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:52:21Z</dc:date>
    <item>
      <title>Request: Example code for LPC11U2X/3X of CDC using USB rom'ed driver.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Request-Example-code-for-LPC11U2X-3X-of-CDC-using-USB-rom-ed/m-p/525212#M7848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larsen on Mon Dec 10 03:19:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We are looking for examples for CDC class using the USB ROM'ed driver for LPC11U2X, LPC11U3X.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We thought it would be simpler to use the Rom'ed drivers than using the nxpUSBlib, but without good examples as a starting point this is not the case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any one with a pointer to some examples?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Request-Example-code-for-LPC11U2X-3X-of-CDC-using-USB-rom-ed/m-p/525212#M7848</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:52:21Z</dc:date>
    </item>
    <item>
      <title>Re: Request: Example code for LPC11U2X/3X of CDC using USB rom'ed driver.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Request-Example-code-for-LPC11U2X-3X-of-CDC-using-USB-rom-ed/m-p/525213#M7849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Tue Dec 11 15:57:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;nxpUSBlib has a switch that forces it to use the USB ROM drivers. It is in the configuration file nxpUSBlibConfig.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;There are also several non-nxpUSBlib source code examples that use the ROM drivers here: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fgfiles%2Fdevper%2Flpc11Uxx" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/gfiles/devper/lpc11Uxx&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Request-Example-code-for-LPC11U2X-3X-of-CDC-using-USB-rom-ed/m-p/525213#M7849</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:52:22Z</dc:date>
    </item>
  </channel>
</rss>