<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1317 doesn't seem to be executing code</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1317-doesn-t-seem-to-be-executing-code/m-p/525072#M7708</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dhames on Fri Sep 27 16:32:51 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everyone.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using an LPC1317 on a board of my own design. I am using LPCXpresso 5.2.6 for compiling, and FlashMagic to program the target MCU via ISP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;FlashMagic programs and verifies the MCU without reporting any problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I power cycle the board after programming, I don't seem to have any code running. I have tried running some of the example projects in LPCXpresso (changing the target to LPC1317) such as systick and blinky, but they all have the same symptoms after programming: all IO pins are logic high and nothing seems to be happening.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;Does this indicate that my user code isn't valid? I have set the target MCU, and FlashMagic should automatically create the required checksum (according to &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsupport.code-red-tech.com%2FCodeRedWiki%2FOutputFormats" rel="nofollow" target="_blank"&gt;http://support.code-red-tech.com/CodeRedWiki/OutputFormats&lt;/A&gt;&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have checked the reset pin on startup and it is staying high, so I don't think it is trying to enter ISP mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions would be greatly appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:56:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:56:35Z</dc:date>
    <item>
      <title>LPC1317 doesn't seem to be executing code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1317-doesn-t-seem-to-be-executing-code/m-p/525072#M7708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dhames on Fri Sep 27 16:32:51 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everyone.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using an LPC1317 on a board of my own design. I am using LPCXpresso 5.2.6 for compiling, and FlashMagic to program the target MCU via ISP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;FlashMagic programs and verifies the MCU without reporting any problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I power cycle the board after programming, I don't seem to have any code running. I have tried running some of the example projects in LPCXpresso (changing the target to LPC1317) such as systick and blinky, but they all have the same symptoms after programming: all IO pins are logic high and nothing seems to be happening.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;Does this indicate that my user code isn't valid? I have set the target MCU, and FlashMagic should automatically create the required checksum (according to &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsupport.code-red-tech.com%2FCodeRedWiki%2FOutputFormats" rel="nofollow" target="_blank"&gt;http://support.code-red-tech.com/CodeRedWiki/OutputFormats&lt;/A&gt;&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have checked the reset pin on startup and it is staying high, so I don't think it is trying to enter ISP mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions would be greatly appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1317-doesn-t-seem-to-be-executing-code/m-p/525072#M7708</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1317 doesn't seem to be executing code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1317-doesn-t-seem-to-be-executing-code/m-p/525073#M7709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sat Sep 28 08:50:30 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Use a debugger...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1317-doesn-t-seem-to-be-executing-code/m-p/525073#M7709</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:56:36Z</dc:date>
    </item>
  </channel>
</rss>