<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LCD 2x16 WINSTAR WH1602A with LPC1769 - something wrong</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-2x16-WINSTAR-WH1602A-with-LPC1769-something-wrong/m-p/524989#M7625</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Tue Oct 14 14:32:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It may not be software at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Have you adjusted the contrast pot?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:10:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:10:46Z</dc:date>
    <item>
      <title>LCD 2x16 WINSTAR WH1602A with LPC1769 - something wrong</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-2x16-WINSTAR-WH1602A-with-LPC1769-something-wrong/m-p/524988#M7624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by teslabox on Mon Oct 13 06:37:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everyone!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to communicate with my LCD display according to HD44780 but probably I do something wrong way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I write C code step by step according the algorithm on page 42:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.sparkfun.com%2Fdatasheets%2FLCD%2FHD44780.pdf" rel="nofollow noopener noreferrer" target="_blank"&gt;https://www.sparkfun.com/datasheets/LCD/HD44780.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I turn on the Vcc one line is lighting.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I run uC with program this line disapears - so it can be good sign but there is no cursor or any char.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
#include "LPC17xx.h"
#include &amp;lt;cr_section_macros.h&amp;gt;
#include &amp;lt;NXP/crp.h&amp;gt;

__CRP const unsigned int CRP_WORD = CRP_NO_CRP; // CRP - Code Read Protection; brak ochrony odczytu kodu

/* Pinout description:
 *
 * Cinfigure lines:
 * pin 4 - RS - GPIO P0.0 (Register Select: 0 - Instruction Register, 1 - Data Register)
 * pin 5 - RW - GPIO P0.1 (Read or Write: 0 - Write to the LCD, 1 - Read from the LCD)
 * pin 6 - EN - GPIO P0.2 (Enable/Clock: Data is latched on falling edge)
 *
 * Data bits lines (only MSB nibble) of 4 bits transmission:
 * pin 11 - DB4 - GPIO P2.0 (bit 0 - LSb)
 * pin 12 - DB5 - GPIO P2.1 (bit 1)
 * pin 13 - DB6 - GPIO P2.2 (bit 2)
 * pin 14 - DB7 - GPIO P2.3 (bit 3 - MSb)
 *
 */

void Timer0_MicroSeconds2 (uint32_t NanoSeconds);// Measured on oscilloscope - 1.0 us, work properly with ABP 100 MHz
void Timer0_MiliSeconds2 (uint32_t MiliSeconds);// Measured on oscilloscope - 1.0 ms, work properly with ABP 100 MHz

// Function of setting GPIO as outputs and RW and EN lines low
void SetPorts (void)
{
// Set all lines as GPIO output
LPC_GPIO2-&amp;gt;FIODIR = ((1&amp;lt;&amp;lt;3)|(1&amp;lt;&amp;lt;2)|(1&amp;lt;&amp;lt;1)|(1&amp;lt;&amp;lt;0));// DATA lines - D0, D1, D2, D3 (4 bits)
LPC_GPIO0-&amp;gt;FIODIR = ((1&amp;lt;&amp;lt;2)|(1&amp;lt;&amp;lt;1)|(1&amp;lt;&amp;lt;0));// Configure lines - RS, RW, EN (3 bits)
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;1);// RW line on the GND all the time - only Write to the LCD
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;2);// EN line low for start as a default state
Timer0_MiliSeconds2 (10);// Delay 10 ms for stable lines
}

// Function of dividing byte on MSB and LSB and send them to the HD44780
void SentLCD (uint8_t Byte)
{
// Send first nibble of the byte - MSB (b7-b4)
// Bus timing values according to Hitachi HD44780 user manual set - Write Operation Figure 25 on page 26
LPC_GPIO0-&amp;gt;FIOSET = (1&amp;lt;&amp;lt;2);// Enable = 1
Timer0_MicroSeconds2 (1);// Delay 1 us (delay 150 ns at least)
LPC_GPIO2-&amp;gt;FIOSET = ((Byte &amp;amp; 0xF0) &amp;gt;&amp;gt; 4);// Byte MSB shifted to LSB place and set on the data lines DB4-DB7
Timer0_MicroSeconds2 (1);// Delay 1 us (delay 80 ns at least)
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;2);// Enable = 0
Timer0_MicroSeconds2 (2);// Delay 2 us (delay 250 ns at least)
// Untill here the MSB (4-bits) were sent to the LCD/HD44780
// The cycle of EN line was HI-2 us and LO-2 us so whole cycle took 2 us

// Send second nibble of byte - LSB
// Bus timing values according to Hitachi HD44780 user manual set - Write Operation Figure 25 on page 26
LPC_GPIO0-&amp;gt;FIOSET = (1&amp;lt;&amp;lt;2);// Enable=1
Timer0_MicroSeconds2 (1);// Delay 1 us (delay 150 ns at least)
LPC_GPIO2-&amp;gt;FIOSET = (Byte &amp;amp; 0x0F);// Byte LSB set on the data lines DB4-DB7
Timer0_MicroSeconds2 (1);// Delay 1 us (delay 80 ns at least)
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;2);// Enable = 0
Timer0_MicroSeconds2 (2);// Delay 2 us (delay 250 ns at least)
// Until here the LSB (4-bits) were sent
// The cycle of EN line was HI-2 us and LO-2 us so whole cycle took again 2 us

// Whole byte sending (MSB + LSB) took 8 us together
}

// Function of the LCD setting and write them to the HD44780
void SetLCD (uint8_t Byte)
{
// Now writing data to the Instruction Register so line RS goes low
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;0);// RS = 0
Timer0_MicroSeconds2 (1);// Delay 1 us (delay 80 ns at least)
//Now when RS line is low configure byte can be send
SentLCD (Byte);// Write data to the HD44780
// Let give 1 ms delay
Timer0_MiliSeconds2 (1);
}

// Function of sending data (chars) to the LCD
void DataLCD (uint8_t Data)
{
// Now writing to the Data Register so line RS goes high
LPC_GPIO0-&amp;gt;FIOSET = (1&amp;lt;&amp;lt;0);// RS = 1
Timer0_MicroSeconds2 (1);// Delay 1us
SentLCD (Data);// Send data to the LCD
}

void StaticTxtLCD (char * s)
{
while (*s)
{
DataLCD (*s);
s++;
}
}

// Function of initializing the LDC
void InitLCD (void)
{
// Reset Function
// Initializing by Internal Reset Circuit
// Hitachi HD44780 user manual, page 23

// Set proper GPIOs for LDC lines
SetPorts ();
// Delay 50 ms for stable lines
Timer0_MiliSeconds2 (50);

// Now writing to the Setting Register so RS line goes low
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;0);// RS = 0
Timer0_MicroSeconds2 (1);// Delay 1 us (delay 80 ns at least)
// Set EN line low as a default value for next steps
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;2);// Enable=0
Timer0_MiliSeconds2 (10);// Delay 10 ms for stable

// Temporary variable for 'for' loop below only
uint8_t i = 0;

// Triple set DB4-DB7 (bits 4-7) as value 0x03 according to HD44780 user manual
for (i = 0; i &amp;lt; 3; i++)
{
LPC_GPIO0-&amp;gt;FIOSET = (1&amp;lt;&amp;lt;2);// Enable = 1
Timer0_MicroSeconds2 (1);// Delay 1 us for EN line proper working
LPC_GPIO2-&amp;gt;FIOSET = (0x03); // Set Data lines as 0x03 value
Timer0_MicroSeconds2 (1);// Delay 1 us for EN line proper working
LPC_GPIO0-&amp;gt;FIOCLR = (1&amp;lt;&amp;lt;2);// Enable = 0
Timer0_MiliSeconds2 (5);// Delay 5ms (should be 4.1 ms at least)
}

Timer0_MiliSeconds2 (50);

// Main settings of the LCD
SetLCD (0x28);// 4-bit transmission, 2 or 4 lines LCD, char 5x8 dots
Timer0_MiliSeconds2 (5);
SetLCD (0x08);// Display Off, Cursor Off, Cursor Toggle Off
Timer0_MiliSeconds2 (5);
SetLCD (0x01);// Clear display
Timer0_MiliSeconds2 (5);
SetLCD (0x06);// Shift characters right (not left), Cursor is moving and window LCD is non-moving
Timer0_MiliSeconds2 (5);
SetLCD (0x0F);// Display On, Cursor On, Cursor Toggle On
Timer0_MiliSeconds2 (5);

Timer0_MiliSeconds2 (50);

}
// Main program
int main (void)
{
// Set the Timer0 for proper delays timing
LPC_SC-&amp;gt;PCONP |= (1&amp;lt;&amp;lt;1); // Set Power On for Timer0
LPC_SC-&amp;gt;PCLKSEL0 |= (1&amp;lt;&amp;lt;2); // Timer0 CLK = APB = 100 MHz (Divider = 1)
LPC_SC-&amp;gt;PCLKSEL0 &amp;amp;=~(1&amp;lt;&amp;lt;3); // Timer0 CLK = APB = 100 MHz (Divider = 1)

// Set GPIO P0.22 as output - there is a LED diode for toggle
LPC_GPIO1-&amp;gt;FIODIR = ((1&amp;lt;&amp;lt;30)|(1&amp;lt;&amp;lt;31));
LPC_GPIO1-&amp;gt;FIOCLR = ((1&amp;lt;&amp;lt;30)|(1&amp;lt;&amp;lt;31));

InitLCD ();
DataLCD (36);

for (;;)
{
LPC_GPIO1-&amp;gt;FIOSET = ((1&amp;lt;&amp;lt;30)|(1&amp;lt;&amp;lt;31));
Timer0_MiliSeconds2 (100);
LPC_GPIO1-&amp;gt;FIOCLR = ((1&amp;lt;&amp;lt;30)|(1&amp;lt;&amp;lt;31));
Timer0_MiliSeconds2 (100);
}

return (0);
}

void Timer0_MicroSeconds2 (uint32_t MicroSeconds)
{
LPC_TIM0-&amp;gt;TCR = 0x02;/* reset timer */
LPC_TIM0-&amp;gt;PR&amp;nbsp; = 0x00;/* set prescaler to zero */
LPC_TIM0-&amp;gt;MR0 = MicroSeconds;
LPC_TIM0-&amp;gt;IR&amp;nbsp; = 0xff;/* reset all interrrupts */
LPC_TIM0-&amp;gt;MCR = 0x04;/* stop timer on match */
LPC_TIM0-&amp;gt;TCR = 0x01;/* start timer */

/* wait until delay time has elapsed */
while (LPC_TIM0-&amp;gt;TCR &amp;amp; 0x01);
}

void Timer0_MiliSeconds2 (uint32_t MiliSeconds)
{
LPC_TIM0-&amp;gt;TCR = 0x02;/* reset timer */
LPC_TIM0-&amp;gt;PR&amp;nbsp; = 0x00;/* set prescaler to zero */
LPC_TIM0-&amp;gt;MR0 = MiliSeconds*100000;
LPC_TIM0-&amp;gt;IR&amp;nbsp; = 0xff;/* reset all interrrupts */
LPC_TIM0-&amp;gt;MCR = 0x04;/* stop timer on match */
LPC_TIM0-&amp;gt;TCR = 0x01;/* start timer */

/* wait until delay time has elapsed */
while (LPC_TIM0-&amp;gt;TCR &amp;amp; 0x01);
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What's wrong? I followed this code many times but I can't find the bug.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-2x16-WINSTAR-WH1602A-with-LPC1769-something-wrong/m-p/524988#M7624</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:45Z</dc:date>
    </item>
    <item>
      <title>Re: LCD 2x16 WINSTAR WH1602A with LPC1769 - something wrong</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-2x16-WINSTAR-WH1602A-with-LPC1769-something-wrong/m-p/524989#M7625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Tue Oct 14 14:32:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It may not be software at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Have you adjusted the contrast pot?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-2x16-WINSTAR-WH1602A-with-LPC1769-something-wrong/m-p/524989#M7625</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:46Z</dc:date>
    </item>
  </channel>
</rss>