<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックClock stability above 60°C</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Clock-stability-above-60-C/m-p/524962#M7598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tbeauchant on Wed May 04 11:27:51 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Folks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm running into an odd issue on a LPC1752 (verified also on a 1751). When the IC package temperature rises above 60°C the clock starts shifting in frequency. I can see this on all my outgoing signals (UART, PWMs, ...) whose timebase gets longer (the UART goes from a steady 115Kbps to about 106Kbps, PWMs are longer by the same amount, ...). This causes mayhem on the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've reproduced the problem on 3 different boards, and also tried replacing the LPC1752 with a 1751 I had in spare and ran into the exact same problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've checked the crystal clock and I am positive the quartz is not causing this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The datasheet seems to say the component is rated +85°C so I'm very surprised by this. If I was to guess, I'd say the PLL in the IC is the root cause.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this a known problem? Has anyone experienced this? Does anyone have an idea for a workaround?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot, any help would be appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:09:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:09:32Z</dc:date>
    <item>
      <title>Clock stability above 60°C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Clock-stability-above-60-C/m-p/524962#M7598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tbeauchant on Wed May 04 11:27:51 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Folks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm running into an odd issue on a LPC1752 (verified also on a 1751). When the IC package temperature rises above 60°C the clock starts shifting in frequency. I can see this on all my outgoing signals (UART, PWMs, ...) whose timebase gets longer (the UART goes from a steady 115Kbps to about 106Kbps, PWMs are longer by the same amount, ...). This causes mayhem on the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've reproduced the problem on 3 different boards, and also tried replacing the LPC1752 with a 1751 I had in spare and ran into the exact same problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've checked the crystal clock and I am positive the quartz is not causing this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The datasheet seems to say the component is rated +85°C so I'm very surprised by this. If I was to guess, I'd say the PLL in the IC is the root cause.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this a known problem? Has anyone experienced this? Does anyone have an idea for a workaround?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot, any help would be appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:09:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Clock-stability-above-60-C/m-p/524962#M7598</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:09:32Z</dc:date>
    </item>
    <item>
      <title>Re: Clock stability above 60°C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Clock-stability-above-60-C/m-p/524963#M7599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Clock-stability-above-60-C/m-p/524963#M7599</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:09:58Z</dc:date>
    </item>
  </channel>
</rss>