<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LpcXpresso - Linked File not compiling</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LpcXpresso-Linked-File-not-compiling/m-p/524958#M7594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Carl-SolderSplash on Mon Apr 22 17:19:11 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Found it,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;It seems LPCxpresso ticks the "Exclude resource from build" option when you import and link a directory into a project, helpful!&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Right click the folder/file you have imported and make sure "Exclude resource from build" is unchecked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:55:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:55:06Z</dc:date>
    <item>
      <title>LpcXpresso - Linked File not compiling</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LpcXpresso-Linked-File-not-compiling/m-p/524957#M7593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Carl-SolderSplash on Mon Apr 22 16:53:40 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hi, A question reguarding project structuring in LpcXpresso, My file structure as follows :&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;MyProj1&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;|- src&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;MyProj2&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;|- src&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;CMSIS&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;|-Cmsis files&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Drivers&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;|-USB&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;|-OtherDrivers&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Shared_Src&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;|-SharedCode1&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have Lpcxpresso projects set up in Myproj1 and Myproj2, linked to CMSIS and compiling.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Now I want to use shared source in the Shared_Src folder between projects, rather than duplicating it. The shared source files are stored outside of the project folder as shown above.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I've done two things, first added it to the include search path, using the following : "${build_project}../../shared_src/" this works and header files in the shared_src can be reference by my project.&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Next I need to use code in the shared_src dir, so I imported it into the project chosing the link option "Create links in workspace" this then adds to the shared_src folder and it's files as links, rather than duplicating them.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;But the code fails to link when calling a function in shared_src from the project.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Any ideas, my goal is to have 1 or more projects share some of the same code. This shared code is configured based upon defines in the project so isn't a standalone lib.&lt;/P&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LpcXpresso-Linked-File-not-compiling/m-p/524957#M7593</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: LpcXpresso - Linked File not compiling</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LpcXpresso-Linked-File-not-compiling/m-p/524958#M7594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Carl-SolderSplash on Mon Apr 22 17:19:11 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Found it,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;It seems LPCxpresso ticks the "Exclude resource from build" option when you import and link a directory into a project, helpful!&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Right click the folder/file you have imported and make sure "Exclude resource from build" is unchecked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LpcXpresso-Linked-File-not-compiling/m-p/524958#M7594</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:55:06Z</dc:date>
    </item>
  </channel>
</rss>