<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question on USB boot mode in a DFU or CDC USB implementation  in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-USB-boot-mode-in-a-DFU-or-CDC-USB-implementation/m-p/524928#M7564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pra18 on Thu Jul 31 08:43:49 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a question w.r.t the DFU usng USB on lpc43xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do we need to use the USB boot mode only if we have a DFU USB implementation in place on my device ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;OR&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Do we need to use the USB boot mode only if we have a CDC USB&amp;nbsp; implementation in place on my device ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen in a ARM9 product that if there is a CDC USB acting as a VirtualCOM one can boot &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;using the USB but with a precondition that there should be a USB cable connected at power up.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;suppose that I have already Serial flash and USART3 boot modes enabled on my platform and I need a USB0 or USB1 &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;boot mode in addition, do I need some special method to achieve booting through USB?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please consider that I dont intend to implement a DFU but would have a CDC USB rather.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What if I would have a CDC class USB in my firmware and will I have to then support USB boot mode in HW.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:53:25 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:53:25Z</dc:date>
    <item>
      <title>Question on USB boot mode in a DFU or CDC USB implementation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-USB-boot-mode-in-a-DFU-or-CDC-USB-implementation/m-p/524928#M7564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pra18 on Thu Jul 31 08:43:49 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a question w.r.t the DFU usng USB on lpc43xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do we need to use the USB boot mode only if we have a DFU USB implementation in place on my device ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;OR&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Do we need to use the USB boot mode only if we have a CDC USB&amp;nbsp; implementation in place on my device ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen in a ARM9 product that if there is a CDC USB acting as a VirtualCOM one can boot &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;using the USB but with a precondition that there should be a USB cable connected at power up.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;suppose that I have already Serial flash and USART3 boot modes enabled on my platform and I need a USB0 or USB1 &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;boot mode in addition, do I need some special method to achieve booting through USB?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please consider that I dont intend to implement a DFU but would have a CDC USB rather.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What if I would have a CDC class USB in my firmware and will I have to then support USB boot mode in HW.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-USB-boot-mode-in-a-DFU-or-CDC-USB-implementation/m-p/524928#M7564</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:53:25Z</dc:date>
    </item>
  </channel>
</rss>