<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1769 SPI clock for receiving (SOLVED)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524897#M7533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Tue Mar 24 00:02:50 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Or to explain things at a slightly higher view point ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;That SPI master clocks out dummy data (usually zeros) after a command send and picks up the returned data&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(on MISO) from the slave (however many bits that you are expecting).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I.e the SPI (as a whole) can be considered as a CIRCULAR shift register with half the bits (MSB) physically in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the master and the other half (LSB) in the slave; but treated as a single item.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Wikipedia SPI has some nice pictures.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;TTFN, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:10:51 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:10:51Z</dc:date>
    <item>
      <title>LPC1769 SPI clock for receiving (SOLVED)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524895#M7531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by otxoasound on Mon Mar 23 10:41:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everybody!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I need to set up communnications using SPI peripheral. The LPC1769 will work as master and an lcd controller (RA8875) as slave. I try an example and SPI works good if I only have to transmit. The LPC1769 does not generate clock after trasnmission of a byte. I need clock generation after transmit because the slave needs clock to send the information the master requests. So I need the same clock cycles as if I were transmitting 16 bits. I try to set 16 bit mode and the slave sends the information, but maybe there is a more elegant way to do it. Somebody could help?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you!!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524895#M7531</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 SPI clock for receiving (SOLVED)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524896#M7532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Mon Mar 23 11:46:44 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: otxoasound&lt;/STRONG&gt;&lt;BR /&gt;I try to set 16 bit mode and the slave sends the information, but maybe there is a more elegant way to do it.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A read / write function as shown in samples :O &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524896#M7532</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 SPI clock for receiving (SOLVED)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524897#M7533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Tue Mar 24 00:02:50 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Or to explain things at a slightly higher view point ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;That SPI master clocks out dummy data (usually zeros) after a command send and picks up the returned data&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(on MISO) from the slave (however many bits that you are expecting).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I.e the SPI (as a whole) can be considered as a CIRCULAR shift register with half the bits (MSB) physically in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the master and the other half (LSB) in the slave; but treated as a single item.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Wikipedia SPI has some nice pictures.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;TTFN, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524897#M7533</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 SPI clock for receiving (SOLVED)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524898#M7534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by otxoasound on Wed Mar 25 03:24:05 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, I am doing it correctly. I have to send dummy data (0x00 is what I actually send) on the MOSI line and meanwhile receive the data from the slave on the MISO line. That is what I actually do, but as I am newbie on SPI communnications, I did not know if I was wrong. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you everybody!!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-SPI-clock-for-receiving-SOLVED/m-p/524898#M7534</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:51Z</dc:date>
    </item>
  </channel>
</rss>