<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックGentle Backdrive on LPC17xx GPIO okay?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Gentle-Backdrive-on-LPC17xx-GPIO-okay/m-p/524889#M7525</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Adam.Garrison on Tue Feb 23 11:24:57 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am looking at the most recent rev of our board and have a question about the inputs on the processor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently we are using a button to power the processer, effectively this pin drives the shutdown pin on our 3.3V regulator. Our charger circuit has a couple inputs/outputs that are fed into the processor for either status or control.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One of the controls the processor can provide is how much current our charger can draw off of USB charging.&amp;nbsp; I currently have a pull up on that pin to Vbus (5V).&amp;nbsp; This trace runs from the charger to a pin on the processor which is an output.&amp;nbsp; In the field I suspect that customers will use the USB Micro B port for charging to keep the battery topped off.&amp;nbsp; The problem I see is this….when they are plugged into USB, but the unit is not turned on, there is 5V on the pin to the processor (through a 10k resistor) which is effectively 500uA of current flowing into that pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked the power pins on the processor and none of them show any voltage at all (&amp;nbsp; I was worried about it backpowering the core through the GPIO pins).&amp;nbsp; The LPC1778 says that it is 5V tolerant when the core is powered.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I limit the current like this, am I okay doing this with such a small amount of current flowing through it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:10:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:10:30Z</dc:date>
    <item>
      <title>Gentle Backdrive on LPC17xx GPIO okay?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Gentle-Backdrive-on-LPC17xx-GPIO-okay/m-p/524889#M7525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Adam.Garrison on Tue Feb 23 11:24:57 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am looking at the most recent rev of our board and have a question about the inputs on the processor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently we are using a button to power the processer, effectively this pin drives the shutdown pin on our 3.3V regulator. Our charger circuit has a couple inputs/outputs that are fed into the processor for either status or control.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One of the controls the processor can provide is how much current our charger can draw off of USB charging.&amp;nbsp; I currently have a pull up on that pin to Vbus (5V).&amp;nbsp; This trace runs from the charger to a pin on the processor which is an output.&amp;nbsp; In the field I suspect that customers will use the USB Micro B port for charging to keep the battery topped off.&amp;nbsp; The problem I see is this….when they are plugged into USB, but the unit is not turned on, there is 5V on the pin to the processor (through a 10k resistor) which is effectively 500uA of current flowing into that pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked the power pins on the processor and none of them show any voltage at all (&amp;nbsp; I was worried about it backpowering the core through the GPIO pins).&amp;nbsp; The LPC1778 says that it is 5V tolerant when the core is powered.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I limit the current like this, am I okay doing this with such a small amount of current flowing through it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Gentle-Backdrive-on-LPC17xx-GPIO-okay/m-p/524889#M7525</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:10:30Z</dc:date>
    </item>
  </channel>
</rss>