<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Burst mode using PWM in LPC1788  in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Burst-mode-using-PWM-in-LPC1788/m-p/524815#M7451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by anuj.tanksali on Wed Feb 24 02:44:21 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I wanted to use burst mode for PWM channel1 in LPC1788&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;burst mode indicates. i want to given fixed no of pulses to PWM&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Once i start the PWM the PWM should stop automatically after the no of pulses are over.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;By stop automatically i mean in should not write any code to stop the PWM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The PWM engine in LPC1788 should stop the PWM automatically after the user specified pulses are complete.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can this be achieved using PWM channel1 in LPC1788&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anuj&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:09:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:09:33Z</dc:date>
    <item>
      <title>Burst mode using PWM in LPC1788</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Burst-mode-using-PWM-in-LPC1788/m-p/524815#M7451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by anuj.tanksali on Wed Feb 24 02:44:21 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I wanted to use burst mode for PWM channel1 in LPC1788&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;burst mode indicates. i want to given fixed no of pulses to PWM&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Once i start the PWM the PWM should stop automatically after the no of pulses are over.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;By stop automatically i mean in should not write any code to stop the PWM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The PWM engine in LPC1788 should stop the PWM automatically after the user specified pulses are complete.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can this be achieved using PWM channel1 in LPC1788&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anuj&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Burst-mode-using-PWM-in-LPC1788/m-p/524815#M7451</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:09:33Z</dc:date>
    </item>
  </channel>
</rss>