<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Lcd controller initialization fail</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lcd-controller-initialization-fail/m-p/524183#M6819</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Sat Jan 16 01:27:14 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i was working on uez product of uezgui-1788-70wvm. it contains LPC1788 interface with 7" WVGA tft capacitive touch screen display. Did&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;initialization of LCD controller registers, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;pin connections assigned,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SDRAM starting address to LCD base address, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;finally enabled LCD and backlight.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;it show full white color means that light was because of backlight right? after that i was tried to write lines display clear but nothing was done. I changed different pen colors also then also i didn't get any pixel variation means color change or something. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;may i know the reason for this state? Sad &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One more thing is Frame buffer address. frame buffer address is LCD base address or local sram memory location ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;in put_pixel function i used ((win-&amp;gt;fb + y * win-&amp;gt;xpsize)[x] = color; ) this instruction at that time this win-&amp;gt;fb need valid address otherwise it wents to hardfault_handler. How can i rectify this bug?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:05:40 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:05:40Z</dc:date>
    <item>
      <title>Lcd controller initialization fail</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lcd-controller-initialization-fail/m-p/524183#M6819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by padmaja on Sat Jan 16 01:27:14 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i was working on uez product of uezgui-1788-70wvm. it contains LPC1788 interface with 7" WVGA tft capacitive touch screen display. Did&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;initialization of LCD controller registers, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;pin connections assigned,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SDRAM starting address to LCD base address, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;finally enabled LCD and backlight.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;it show full white color means that light was because of backlight right? after that i was tried to write lines display clear but nothing was done. I changed different pen colors also then also i didn't get any pixel variation means color change or something. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;may i know the reason for this state? Sad &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One more thing is Frame buffer address. frame buffer address is LCD base address or local sram memory location ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;in put_pixel function i used ((win-&amp;gt;fb + y * win-&amp;gt;xpsize)[x] = color; ) this instruction at that time this win-&amp;gt;fb need valid address otherwise it wents to hardfault_handler. How can i rectify this bug?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks &amp;amp; regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;padmaja.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lcd-controller-initialization-fail/m-p/524183#M6819</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:05:40Z</dc:date>
    </item>
  </channel>
</rss>