<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [Solved]USBD: Multiple instances ? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Solved-USBD-Multiple-instances/m-p/524094#M6730</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by chris_bayley_trimble on Tue Apr 14 16:52:38 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When using a 4370 is there any known reason I can't use multiple instances of USBD ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a setup that should be able use both USB0 and USB1 as devices, and either one works fine on it own but if I call &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;USBD_API-&amp;gt;hw-&amp;gt;Init() twice (with different instance variables of course) the stack appears to jam up.(Interrupts become intermittent/dropped and the device does not enummerate)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there some known thing I should be aware of ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:48:08 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:48:08Z</dc:date>
    <item>
      <title>[Solved]USBD: Multiple instances ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Solved-USBD-Multiple-instances/m-p/524094#M6730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by chris_bayley_trimble on Tue Apr 14 16:52:38 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When using a 4370 is there any known reason I can't use multiple instances of USBD ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a setup that should be able use both USB0 and USB1 as devices, and either one works fine on it own but if I call &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;USBD_API-&amp;gt;hw-&amp;gt;Init() twice (with different instance variables of course) the stack appears to jam up.(Interrupts become intermittent/dropped and the device does not enummerate)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there some known thing I should be aware of ??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Solved-USBD-Multiple-instances/m-p/524094#M6730</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: [Solved]USBD: Multiple instances ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Solved-USBD-Multiple-instances/m-p/524095#M6731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by chris_bayley_trimble on Wed Apr 15 16:44:09 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Got it:&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;USBD_API_INIT_PARAM_T::mem_base must be 2048 byte aligned.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;: )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:48:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Solved-USBD-Multiple-instances/m-p/524095#M6731</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:48:09Z</dc:date>
    </item>
  </channel>
</rss>