<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: The EMC clock limitation</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523949#M6585</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Mon Jan 05 09:42:29 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Mori_64,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Maximum data transfer speed with SDRAM is also limited by the speed of the IO. So, either you can run device at core frequency of 80MHz and SDRAM clock at 80MHz or you can run core at 120MHz and SDRAM at 60MHz.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:06:13 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:06:13Z</dc:date>
    <item>
      <title>The EMC clock limitation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523948#M6584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Mori_64 on Mon Jan 05 08:06:49 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As i see in lpc1788 user manual :&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Clock: The EMC clock can be the same as the CPU clock (the default), or half that. &lt;BR /&gt;The lower rate is intended to be used primarily when the CPU is running faster than &lt;BR /&gt;the external bus can support. Clock selection for the EMC is described in &lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;but is there any limitation ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;for example can i use sd_ram in 120 Mhz ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523948#M6584</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: The EMC clock limitation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523949#M6585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Mon Jan 05 09:42:29 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Mori_64,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Maximum data transfer speed with SDRAM is also limited by the speed of the IO. So, either you can run device at core frequency of 80MHz and SDRAM clock at 80MHz or you can run core at 120MHz and SDRAM at 60MHz.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523949#M6585</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: The EMC clock limitation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523950#M6586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Mori_64 on Tue Jan 06 06:54:55 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi mc&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your replay .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tested my sd_ram with 120Mhz and it works fine !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523950#M6586</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:06:14Z</dc:date>
    </item>
    <item>
      <title>Re: The EMC clock limitation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523951#M6587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Tue Jan 06 16:48:04 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It may &lt;/SPAN&gt;&lt;I&gt;be working fine&lt;/I&gt;&lt;SPAN&gt; at the temperatures on the testing bench and with the voltage and power&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;that were used in your (limited? simple?) tests, but you are are running at &lt;/SPAN&gt;&lt;STRONG&gt;150% over the rated &lt;I&gt;guaranteed&lt;/I&gt; specification!&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;On long term running or when different operating characterists apply, you won't have any come-back.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;I&gt;Any form of over-clocking&lt;/I&gt;&lt;SPAN&gt; is entirely at your own risk.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This may not concern you for hobby projects, but such practice is totaly unacceptable in any commercial enterprises.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As the saying goes ... you have been warned.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EDIT: you need to read the &lt;/SPAN&gt;&lt;I&gt;data sheet&lt;/I&gt;&lt;SPAN&gt; for the part for limits etc. not the generic user manual for the family.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523951#M6587</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:06:14Z</dc:date>
    </item>
    <item>
      <title>Re: The EMC clock limitation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523952#M6588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Wed Jan 07 08:26:11 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike is right. Even if the memory interface in this chip is quite robust with regards to overclocking, running it on 120MHz is at your own risk.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;At least you need to run a stress test over the possible voltage and temperature range. Lower voltage and higher temperature is the worst case for this test.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support Team.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-EMC-clock-limitation/m-p/523952#M6588</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:06:15Z</dc:date>
    </item>
  </channel>
</rss>