<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Auto detect DEVICE/HOST mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523885#M6521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fariouche on Mon Nov 12 14:41:18 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm currently using the new usblib 0.98 with an lpc1769 (lpcxpresso)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to use Device and Host. Currently I've setup the controller as a CDC device and it work great.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now, I can switch to Host mode manually (as described in the sample), but looking at the doc, I've seen that the lib can switch automatically depending on the UID pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How can I use this feature? If I understood correctly, EVENT_USB_UIDChange should fire up in that case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But I doubt it works as I do not see any reference to this function in the library except in a .h file!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Fariouche&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:46:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:46:30Z</dc:date>
    <item>
      <title>Auto detect DEVICE/HOST mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523885#M6521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fariouche on Mon Nov 12 14:41:18 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm currently using the new usblib 0.98 with an lpc1769 (lpcxpresso)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to use Device and Host. Currently I've setup the controller as a CDC device and it work great.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now, I can switch to Host mode manually (as described in the sample), but looking at the doc, I've seen that the lib can switch automatically depending on the UID pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How can I use this feature? If I understood correctly, EVENT_USB_UIDChange should fire up in that case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But I doubt it works as I do not see any reference to this function in the library except in a .h file!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Fariouche&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523885#M6521</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: Auto detect DEVICE/HOST mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523886#M6522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fariouche on Fri Nov 16 14:13:08 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I got the answer: This is an OTG feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have to found an other way I think :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523886#M6522</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: Auto detect DEVICE/HOST mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523887#M6523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpUSBlib team on Mon Nov 26 10:15:04 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes the UID is an input to an external OTG PHY that you would need to add to your design.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A much simpler and cheaper method would be to use a GPIO input.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Auto-detect-DEVICE-HOST-mode/m-p/523887#M6523</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:46:31Z</dc:date>
    </item>
  </channel>
</rss>