<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Emwin NOT working properly with SSD 1963 in 8 bit mode. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Emwin-NOT-working-properly-with-SSD-1963-in-8-bit-mode/m-p/523848#M6484</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wouter on Tue Oct 29 08:00:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Akshay,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;I just responded to your other thread (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fcan-we-configure-emwin-16-bit-data-transfer-our-8-bit-data-lines" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/can-we-configure-emwin-16-bit-data-transfer-our-8-bit-data-lines&lt;/A&gt;&lt;SPAN&gt;). In the future please try avoid opening multiply threads on the same subject.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;By the looks of your code, the low-level routines are not according to spec, and the 18bpp mode you selected in the init functions is not supported by the emWin driver. If you fix those two issues, you just might be lucky and have a working LCD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Wouter&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:03:28 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:03:28Z</dc:date>
    <item>
      <title>Emwin NOT working properly with SSD 1963 in 8 bit mode.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Emwin-NOT-working-properly-with-SSD-1963-in-8-bit-mode/m-p/523847#M6483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by AkshayHV on Sat Oct 26 06:44:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi i am interfacing a 4.3 inch TFT with LPC1768 ,the controller in the display is SSD1963&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;it is basically a parallel 8 bit interface but the problem is even though the interface is of 8 bit in the SSD_init() function if i am sending a command to say it is 8 bit interface my display is not working properly but if i configure it as 9 bit interface it is working for some of the GUI in emwin but for some GUI's the colors are not displaying as normal &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks and regards &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Akshay H V&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Emwin-NOT-working-properly-with-SSD-1963-in-8-bit-mode/m-p/523847#M6483</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: Emwin NOT working properly with SSD 1963 in 8 bit mode.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Emwin-NOT-working-properly-with-SSD-1963-in-8-bit-mode/m-p/523848#M6484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wouter on Tue Oct 29 08:00:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Akshay,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;I just responded to your other thread (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fcan-we-configure-emwin-16-bit-data-transfer-our-8-bit-data-lines" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/can-we-configure-emwin-16-bit-data-transfer-our-8-bit-data-lines&lt;/A&gt;&lt;SPAN&gt;). In the future please try avoid opening multiply threads on the same subject.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;By the looks of your code, the low-level routines are not according to spec, and the 18bpp mode you selected in the init functions is not supported by the emWin driver. If you fix those two issues, you just might be lucky and have a working LCD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Wouter&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:03:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Emwin-NOT-working-properly-with-SSD-1963-in-8-bit-mode/m-p/523848#M6484</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:03:28Z</dc:date>
    </item>
  </channel>
</rss>