<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックADC input structure</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-input-structure/m-p/514341#M641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by br1 on Tue Feb 16 03:21:40 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need the input structure and acquisition time of the 12 bit ADC on LPC1518 series.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The aim is to simulate the maximum source resistance (and sampling rate) I can connect to the ADC versus a tolerable offset error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the ADC1_1 input in burst mode at maximum sampling rate (50MHz ADC clock).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I run a spice simulation with the data I found on the datasheet, or presumed, but it doesn't coincide with the prototype results.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Specifically I used:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* 0.32 pF ADC input capacitance (Cia) from Fig. 39 of datasheet&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* 5 to 25 ohm multiplexer resistance (Rsw) from Fig. 39 of datasheet&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* I assumed 13 cycles acquisition time and 12 cycles conversion time (user manual specify only 25 cycles overall)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* I assumed Cia charged to Vref or Vref/2 between every sample (because I saw a positive offset with a grounded input).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* I omitted Cdac from Fig. 39 of datasheet because not specified nor the other end connected&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the values as in the attached picture I get 8 mV of offset (from a grounded input) while actually I measured 60 mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems the Cia is an order of magnitude higher than what specified or Cdac influences the circuit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What am I missing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;TIA,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Bruno&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:13:05 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:13:05Z</dc:date>
    <item>
      <title>ADC input structure</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-input-structure/m-p/514341#M641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by br1 on Tue Feb 16 03:21:40 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need the input structure and acquisition time of the 12 bit ADC on LPC1518 series.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The aim is to simulate the maximum source resistance (and sampling rate) I can connect to the ADC versus a tolerable offset error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the ADC1_1 input in burst mode at maximum sampling rate (50MHz ADC clock).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I run a spice simulation with the data I found on the datasheet, or presumed, but it doesn't coincide with the prototype results.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Specifically I used:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* 0.32 pF ADC input capacitance (Cia) from Fig. 39 of datasheet&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* 5 to 25 ohm multiplexer resistance (Rsw) from Fig. 39 of datasheet&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* I assumed 13 cycles acquisition time and 12 cycles conversion time (user manual specify only 25 cycles overall)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* I assumed Cia charged to Vref or Vref/2 between every sample (because I saw a positive offset with a grounded input).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* I omitted Cdac from Fig. 39 of datasheet because not specified nor the other end connected&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the values as in the attached picture I get 8 mV of offset (from a grounded input) while actually I measured 60 mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems the Cia is an order of magnitude higher than what specified or Cdac influences the circuit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What am I missing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;TIA,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Bruno&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-input-structure/m-p/514341#M641</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:13:05Z</dc:date>
    </item>
  </channel>
</rss>