<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックFast Flash Programming via Bootloader</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fast-Flash-Programming-via-Bootloader/m-p/523733#M6369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Tue Nov 13 04:22:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;As you might know, the boot rom in LPC177x/8x is limited to 56K baudrate, running with the 12MHz internal oscillator.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In production, this might take a big amount of time for programming the internal flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, it is possible to load a small programm into the internal RAM of the CPU which sets the baudrate&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to a higher value.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The appended program boot_setbaud.c sets the baudrate to 115K. It is position independent.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You have to use the commands W(rite), U(nlock) and (G)o. The return string of&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the G(o) command is crippled because of the switched baudrate. After this, you can&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;switch the PC to 115K.&lt;/SPAN&gt;&lt;BR /&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338099"&gt;boot_setbaud.tar.gz&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338099"&gt;boot_setbaud.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:03:36 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:03:36Z</dc:date>
    <item>
      <title>Fast Flash Programming via Bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fast-Flash-Programming-via-Bootloader/m-p/523733#M6369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Tue Nov 13 04:22:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;As you might know, the boot rom in LPC177x/8x is limited to 56K baudrate, running with the 12MHz internal oscillator.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In production, this might take a big amount of time for programming the internal flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, it is possible to load a small programm into the internal RAM of the CPU which sets the baudrate&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to a higher value.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The appended program boot_setbaud.c sets the baudrate to 115K. It is position independent.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You have to use the commands W(rite), U(nlock) and (G)o. The return string of&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the G(o) command is crippled because of the switched baudrate. After this, you can&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;switch the PC to 115K.&lt;/SPAN&gt;&lt;BR /&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338099"&gt;boot_setbaud.tar.gz&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338099"&gt;boot_setbaud.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Fast-Flash-Programming-via-Bootloader/m-p/523733#M6369</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:03:36Z</dc:date>
    </item>
  </channel>
</rss>