<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB ROM API - How to deinit USB ROM Code?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-ROM-API-How-to-deinit-USB-ROM-Code/m-p/523641#M6277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cneubert on Mon Jan 11 07:29:01 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In my application I can send a command over USB and then my application will jump to my bootloader. In my bootloader I also want to be able to receive commands over USB, but I can´t get it working this way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a bootloader which can receive commands over USB (this works without flaws). The bootloader jumps to my application and there I can also receive commands over USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But when I then jump from my application to my bootloader, USB wont work anymore. Windows reports me an USB device which is not identified.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So every part of my bootloader works if I jump from my application back to it, but not USB. USB is working when I power up my device and the bootloader first starts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So I think that I miss something when deiniting USB when I jump from my application to my bootloader. Although it seems it doesn´t matter when jumping from bootloader to application as USB there is working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have an idea what´s wrong? Has anyone implemented USB in his bootloader and also in his application?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:46:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:46:06Z</dc:date>
    <item>
      <title>USB ROM API - How to deinit USB ROM Code?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-ROM-API-How-to-deinit-USB-ROM-Code/m-p/523641#M6277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cneubert on Mon Jan 11 07:29:01 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In my application I can send a command over USB and then my application will jump to my bootloader. In my bootloader I also want to be able to receive commands over USB, but I can´t get it working this way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a bootloader which can receive commands over USB (this works without flaws). The bootloader jumps to my application and there I can also receive commands over USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But when I then jump from my application to my bootloader, USB wont work anymore. Windows reports me an USB device which is not identified.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So every part of my bootloader works if I jump from my application back to it, but not USB. USB is working when I power up my device and the bootloader first starts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So I think that I miss something when deiniting USB when I jump from my application to my bootloader. Although it seems it doesn´t matter when jumping from bootloader to application as USB there is working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have an idea what´s wrong? Has anyone implemented USB in his bootloader and also in his application?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-ROM-API-How-to-deinit-USB-ROM-Code/m-p/523641#M6277</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:46:06Z</dc:date>
    </item>
  </channel>
</rss>