<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1758 Interrupt IN endpoint does not retire blank DMA descriptors</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-Interrupt-IN-endpoint-does-not-retire-blank-DMA/m-p/523577#M6213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ejg on Wed Jan 27 03:58:25 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm running my LPC1758 as a USB device and sending data to the host over a bulk IN endpoint and an interrupt IN endpoint. In both cases the length of the data I'm sending is equal to the maximum packet size of the endpoint.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The user manual states that:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;If the last buffer length completes on a MaxPacketSize packet boundary, the device software must program the next DD with DMA_buffer_length field 0, so that an empty packet is sent by the device to mark the end of the USB transfer for the host.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The weird thing is on the bulk endpoint these empty DMA descriptors will have their status set to retired, the interrupt endpoint doesn't retire them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've managed to fudge the code together to get everything working, just wondered if anyone understood why this is happening?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:45:05 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:45:05Z</dc:date>
    <item>
      <title>LPC1758 Interrupt IN endpoint does not retire blank DMA descriptors</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-Interrupt-IN-endpoint-does-not-retire-blank-DMA/m-p/523577#M6213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ejg on Wed Jan 27 03:58:25 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm running my LPC1758 as a USB device and sending data to the host over a bulk IN endpoint and an interrupt IN endpoint. In both cases the length of the data I'm sending is equal to the maximum packet size of the endpoint.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The user manual states that:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;If the last buffer length completes on a MaxPacketSize packet boundary, the device software must program the next DD with DMA_buffer_length field 0, so that an empty packet is sent by the device to mark the end of the USB transfer for the host.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The weird thing is on the bulk endpoint these empty DMA descriptors will have their status set to retired, the interrupt endpoint doesn't retire them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've managed to fudge the code together to get everything working, just wondered if anyone understood why this is happening?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1758-Interrupt-IN-endpoint-does-not-retire-blank-DMA/m-p/523577#M6213</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:45:05Z</dc:date>
    </item>
  </channel>
</rss>