<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1768 SPI Test Mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523518#M6154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cfbsoftware on Tue Nov 19 14:30:12 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;My reading of the documentation is that you should set the bitfield 7:1 to the value 1, not to set all bits 7:1 to 1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Try LPC_SPI-&amp;gt;SPTCR = 0x02;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:01:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:01:30Z</dc:date>
    <item>
      <title>LPC1768 SPI Test Mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523517#M6153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ddink on Tue Nov 19 09:21:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need a continious SPI clock in master mode (running all the time, even if there's nothing&amp;nbsp; to send) for testing purposes. I like to generate this by using the SPI test mode. Therefore I added SPTCR to the LP17xx.h Cmsis library:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;typedef struct
{
&amp;nbsp; __IO uint32_t SPCR;
&amp;nbsp; __I&amp;nbsp; uint32_t SPSR;
&amp;nbsp; __IO uint32_t SPDR;
&amp;nbsp; __IO uint32_t SPCCR;
&amp;nbsp; __IO uint32_t SPTCR;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t RESERVED0[2];
&amp;nbsp; __IO uint32_t SPINT;
} LPC_SPI_TypeDef;&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;then I added &lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;LPC_SPI-&amp;gt;SPTCR = 0x0FE;&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;SPAN&gt;to the runtime code (after the SPI was initialized).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the disassembly it looks as following:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt; 23e:f04f 0300 mov.wr3, #0
 242:f2c4 0302 movtr3, #16386; 0x4002
 246:f04f 02fe mov.wr2, #254; 0xfe
 24a:611a&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; strr2, [r3, #16]&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;All good so far, but when I run the program and read the SPTCR register, it is empty. There is also no cont. clock on the SPI Clk pin. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Are there any restritions for the testing mode or am I doing anythin wrong?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you very much!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ddink&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523517#M6153</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:01:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 SPI Test Mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523518#M6154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cfbsoftware on Tue Nov 19 14:30:12 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;My reading of the documentation is that you should set the bitfield 7:1 to the value 1, not to set all bits 7:1 to 1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Try LPC_SPI-&amp;gt;SPTCR = 0x02;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523518#M6154</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:01:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 SPI Test Mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523519#M6155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ddink on Thu Nov 21 01:16:56 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you very much for your reply! I tried it with 7:1 as 1 (with the following disassembly:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt; 23e:f04f 0300 mov.wr3, #0
 242:f2c4 0302 movtr3, #16386; 0x4002
 246:f04f 0202 mov.wr2, #2
 24a:611a&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; strr2, [r3, #16]&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Still no continious clock&amp;nbsp; :~ &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-SPI-Test-Mode/m-p/523519#M6155</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:01:30Z</dc:date>
    </item>
  </channel>
</rss>